2017-08-05 1:44 AM
Hello!
I Have a Problem:
I want to transmit Midi signals using my Discovery board in DMA mode because I need the processing power during the transfer. Midi is based on UART meaning I am using the UART Peripheral. When I transfer a data chain the Data using Polling I can send out another Data chain directly afterwards. But when I use DMA and transfer a Data chain I have to wait about a 5th of a second before another one can be sent. And I need to be able to instantly send another chain of data if I have to. As a reference I am using the Preconfigured Initialization code generated by the Cube MX Hal.I would really appriciate it if someone could help me speed the DMA post processing or whatever is happening up. I wouldn't even know why such extensive post processing would need to happen. 1/5th of a second is quite a lot.
Greetings and Thanks
Henrik
#stm32f4-discovery #polling #time #uart-dma #uart-tx2017-08-05 4:14 AM
But when I use DMA and transfer a Data chain I have to wait about a 5th of a second before another one can be sent
How do you mean thart you wait? What happens if you don't wait?
JW
2017-08-05 7:21 AM
Sequencing in HAL? Not sure where it would pull 200ms of delay
I've posted examples using SPL which chain multiple strings continuously, with no inter-symbol gaps, so pretty sure if you use the DMA TC interrupt you can restart a new transaction transparently.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.