2014-11-09 2:41 PM
Hi!
I have stm32f4 discovery board MB997C. I`m trying to communicate with LIS3DSH accelerometer. I have a problem - MISO line (port PA6) is always high. I`m just trying to get the value of WHO_AM_I register and as response I always get 0xFF. Here is my configuration code:
#define CS_HIGH GPIO_SetBits(GPIOE, GPIO_Pin_3)
#define CS_LOW GPIO_ResetBits(GPIOE, GPIO_Pin_3)GPIO_InitTypeDef GPIOA_InitStructure;
GPIO_InitTypeDef GPIOE_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; SPI_InitTypeDef SPI_InitStructure;uint8_t receivedByte;
unsigned int TransactionFlag = 0x0000; unsigned int TransmitCounter = 0x0000;void main(void)
{ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOE, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE); GPIOA_InitStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7; GPIOA_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIOA_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIOA_InitStructure.GPIO_OType = GPIO_OType_PP; GPIOA_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIOA_InitStructure); GPIO_PinAFConfig(GPIOA,GPIO_PinSource5,GPIO_AF_SPI1); GPIO_PinAFConfig(GPIOA,GPIO_PinSource6,GPIO_AF_SPI1); GPIO_PinAFConfig(GPIOA,GPIO_PinSource7,GPIO_AF_SPI1); GPIOE_InitStructure.GPIO_Pin = GPIO_Pin_3; GPIOE_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIOE_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIOE_InitStructure.GPIO_OType = GPIO_OType_PP; GPIOE_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOE, &GPIOE_InitStructure); CS_HIGH; SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_High; SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft | SPI_NSSInternalSoft_Set; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_64; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_Init(SPI1, &SPI_InitStructure); NVIC_PriorityGroupConfig(NVIC_PriorityGroup_2); NVIC_InitStructure.NVIC_IRQChannel = SPI1_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); SPI_Cmd(SPI1, ENABLE); // SPI_I2S_ITConfig(SPI1, SPI_I2S_IT_RXNE, ENABLE); // SPI_I2S_ITConfig(SPI1, SPI_I2S_IT_TXE, ENABLE); while(1) { unsigned long i;CS_LOW;
for(i = 0; i < 10; i++); SPI_I2S_SendData(SPI1, 0x8F); //Wait for transmission to complete while (!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE)); //Wait for received data to complete while (!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE)); //Wait for SPI to be ready // while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_BSY)); receivedByte = SPI_I2S_ReceiveData(SPI1); SPI_I2S_SendData(SPI1, 0x00); //Wait for transmission to complete while (!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE)); //Wait for received data to complete while (!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE)); receivedByte = SPI_I2S_ReceiveData(SPI1); //Wait for transmission to complete // while (!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE)); //Wait for SPI to be ready // while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_BSY)); for(i = 0; i < 10; i++); CS_HIGH;for(i = 0; i < 100; i++);
} } Help me please, what am i doing wrong?2018-02-23 9:10 AM
Can you run just blink on PA6?
2018-02-23 9:21 AM
My code with StdPeriph:
#include 'stm32f4xx.h'
#include 'main.h'
#include 'spi.h'
#define LIS3DSH
#define LIS3DSH_OUT_X_L 0x28
#define LIS3DSH_OUT_X_H 0x29
#define LIS3DSH_OUT_Y_L 0x2a
#define LIS3DSH_OUT_Y_H 0x2b
#define LIS3DSH_OUT_Z_L 0x2c
#define LIS3DSH_OUT_Z_D 0x2c
#define HYSTERESIS 6000
int16_t AxisX = 0;
int16_t AxisY = 0;
//int16_t AxisZ = 0;
uint8_t temp_x_l = 0;
uint8_t temp_x_h = 0;
uint8_t temp_y_l = 0;
uint8_t temp_y_h = 0;
uint8_t writeData(uint8_t data)
{
while(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_BSY) == SET) ;
SPI_I2S_SendData(SPI1, data);
while(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_BSY) == SET) ;
return SPI_I2S_ReceiveData(SPI1);
}
int getReg(uint8_t address)
{
uint8_t data=0;
address|=(1<<7);
GPIO_ResetBits(GPIOE,GPIO_Pin_3);
writeData(address);
data = writeData(0x00);
GPIO_SetBits(GPIOE,GPIO_Pin_3);
return data;
}
void setReg(uint8_t address, uint8_t value)
{
GPIO_ResetBits(GPIOE,GPIO_Pin_3);
writeData(address);
writeData(value);
GPIO_SetBits(GPIOE,GPIO_Pin_3);
}
int main(void)
{
Led_init();
SPI_init();
// getReg(0x0f); // get ID
setReg(0x20, 0x97);
setReg(0x23, 0xA0);
while(1)
{
temp_x_h = getReg(LIS3DSH_OUT_X_H);
temp_x_l = getReg(LIS3DSH_OUT_X_L);
temp_y_h = getReg(LIS3DSH_OUT_Y_H);
temp_y_l = getReg(LIS3DSH_OUT_Y_L);
AxisX = (temp_x_h) << 8 | temp_x_l;
AxisY = (temp_y_h) << 8 | temp_y_l;
if (AxisX > HYSTERESIS)
{ R_ON(); }
else if (AxisX < -HYSTERESIS)
{ G_ON(); }
else
{ R_OFF();
G_OFF(); }
if (AxisY > HYSTERESIS)
{ Y_ON(); }
else if (AxisY < -HYSTERESIS)
{ B_ON(); }
else
{ B_OFF();
Y_OFF(); }
}
}
2018-02-23 9:24 AM
I would try the MEMS example from the F4 disco firmware package.
I used to start my project with working examples, and added my code then later.
And the example would be a good functional test.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.