2013-01-07 6:18 PM
I am trying to get the F4 discovery board to communicate with a FPGA board via the FSMC but I am having some problems.
I have connected the data 0-15 lines, we, oe, and addr 16-23 from the discovery to my fpga. I can get the data to output correctly and read it on the fpga, but the problem is with the address lines. They do not seem to be sending the address that I want them to and I don't think that I fully understand how to get them to send the address that I want. Right now I am using the following to write data on the upper (16-23) bits of the address line. __IO uint32_t * MYBASE4 = ((uint32_t)(0x600A0000)); I think that this should be accessing address 10 but it does not. I write data to it with this *MYBASE4 = 567; This puts 567 on the data lines and the FPGA reads it correctly. Any help on what I am missing with the address lines would be appreciated. Dave2013-01-07 7:34 PM
I might expect you see 0x5, in 16-bit mode A16 (ext) will be A17 (int) as the STM32 shifts the address (A0 being meaningless in a 16-bit context), as I recall.
2013-01-08 4:11 AM
Also, there will be two consecutive writes to the same address (as A0 is unconnected), if a whole word (uint32_t) is written.
JW2013-01-08 5:46 AM
I have tried doing the following
__IO uint32_t * MYBASE7 = ((uint32_t)(0x68000000 | (10<<17))); But I still don't see a 10 for address, but are you saying that I should also ignore A16 and start at A17 on my wiring and use a 7 bit bus? Also how can I only do a single write and not a double (32bit) write? Thanks Dave2013-01-08 6:35 AM
> But I still don't see a 10 for address,
And what do you see? > but are you saying that I should also ignore A16 and start at A17 on my wiring and use a 7 bit bus? No. Read the fine manual, chapter 32.4.1 > Also how can I only do a single write and not a double (32bit) write? uint16_t * JW2013-01-08 7:18 AM
>> But I still don't see a 10 for address,
>And what do you see? I have not been able to get a good reading on my scope yet. > >but are you saying that I should also ignore A16 and start at A17 on my wiring and use a 7 bit bus? >No. Read the fine manual, chapter 32.4.1 I have read that section a few times but I am not sure what I am missing in it. In this section it says 1. In case of a 16-bit external memory width, the FSMC will internally use HADDR[25:1] to generate the address for external memory FSMC_A[24:0]. Whatever the external memory width (16-bit or 8-bit), FSMC_A[0] should be connected to external memory address A[0]. So I think my code should be working but I don't get what I am missing. I cannot connect my address starting at A[0] since that is not broken out on my board. >> Also how can I only do a single write and not a double (32bit) write? >uint16_t * So I should change it like this? __IO uint16_t * MYBASE7 = ((uint16_t)(0x60000000 | (10<<16))); I also see that a lot of LCD examples on the discovery board start with base address 0x68000000, is that because they are using something in the upper address lines to trigger some other function on the LCD? Thanks Dave2013-01-08 5:04 PM
Well I got it working
The following changes made everything work as I needed Address __IO uint32_t * FPGA = ((uint32_t)(0x60000000) | (address<<17)); Write *FPGA = (uint16_t)data; Dave2013-01-08 5:20 PM
Well I got it working
The following changes made everything work as I needed Address __IO uint32_t * FPGA = ((uint32_t)(0x60000000) | (address<<17)); Write *FPGA = (uint16_t)data; DaveWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.