2023-03-02 5:13 PM
2023-03-02 8:23 PM
What is TRG1/TRG2?
JW
2023-03-04 8:41 AM
Sorry, was referring to the trigger output of timers 1 and 2, should have been TRGO1 and TRGO2. The question is can a single general purpose timer be configured to be both a slave and master simultaneously.
2023-03-04 12:39 PM
Yes, timer can be slave and master simultaneously. Read also carefuly section about "Master/Slave mode" (MSM bit) in reference manual.
2023-03-06 9:25 AM
Michael, will do, thanks for your help.
2023-03-06 9:40 AM
Should be tables in the Reference Manual (RM0090)
TIM1->TRGO --> TIM2 ITR0
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.