2014-03-30 9:34 AM
Hello,
at first, I try to explain my target functinality: -TIM1 generates a 3PH Center aligned PWM - the ADCs are configured in triple mode, some channels are converted and the DMA generates an Interrupt when the Transfer of data to RAM has finished (regular channels) -TIM1 should Trigger the sampling sequence of the ADCs when 0, Period, or both (Software selectable) What is working: -the timer is configured proper an generates the PWM pattern -the ADCs and DMA work, but only with Software Trigger The question: Is it possible to configure TIM1 to generate the Trigger for the ADCs in that way? The Statements ''TIM1_CHx Event'' in RM0090 on page 396 are not clear to me. It seems to me, that a new conversion is immediately started, after the last has finnished. Thanks in advance for your help! #adc #trog #triple-mode #dma2014-03-30 2:47 PM
Triple mode implies they all trigger at the same time, some how I think you want them phase aligned with the respective channels.
You should be able to configure each of the three ADC with a different channel, and different trigger TIM1_CH1, TIM1_CH2_ TIM1_CH3, and you'll need three independent DMA, or IRQ2014-03-30 9:21 PM
Hi Clive,
the three PWM-Channels are running with no Phase shift, simmilar to the Picture (sorry for Picture source, Google did it ;) :( I want all regular ADC channels on all ADCs converted at PWM Counter == 0, Counter == ADD or both. When does the ''TIM1_CHx Event'' Trigger the ADC? I can't find further Information for this Events... Is it right, that the Trigger for triple mode ADC are only the ADC1 ones?2014-03-31 6:08 AM
You should be able to start the conversion on multiple channels using the trigger. You only have a single trigger, although you can presumably reconfigure it on the fly.
The conversions on an ADC will occur one after another at the sampling rate, in non-continuous mode it will stop after the list is enumerated. In Triple mode the triggering is mastered by ADC1, but you really want all the ADC configured in a balanced fashion. In this mode you get 3 channels sampled in a synchronous fashion. For a TIM1 Channel1 Trigger, it should occur when TIM1->CNT == TIM1->CCR1We’re moving the ST Community to a new platform to give you a better and more reliable community experience.