2015-06-24 7:11 AM
2015-06-24 7:52 AM
It helps to read the fine print in the Reference Manual, especially when the author anticipated your reaction with a typo.
''DAM mode 2 is used in interleaved mode and in regular simultaneous mode (for Dual ADC mode only).'' Cheers, Hal2015-06-24 10:13 AM
Dear Hal,
Thank you very much for your answer, but I didn't really get it. I had seen that part and I thought of it as if I can use DMA mode 2 in Triple ADC mode however I want, but in Dual ADC mode only in interleaved and regular simultaneous mode. And actually exactly above the part you mentioned with the nice typo :) it says how the DMA requests are generated in Triple mode. Excuse me if I mixed it up. Regards, PantelisWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.