2015-05-11 4:14 AM
Hello, I have some problem with USART2 (stm32f373). USART1 is working with same code but, Usart2 does not work. here is the code.
void Uart_Int(void) { GPIO_InitTypeDef GPIO_InitStructure; USART_InitTypeDef USART_InitStructure; USART_ClockInitTypeDef USART_ClockInitStructure; USART_ClockStructInit(&USART_ClockInitStructure); USART_ClockInit(USART2, &USART_ClockInitStructure); RCC_APB2PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA , ENABLE); GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_7); GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_7); GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;//--------- GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;//--------- GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3; GPIO_Init(GPIOA, &GPIO_InitStructure); USART_InitStructure.USART_BaudRate =9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART2, &USART_InitStructure); USART_Cmd(USART2, ENABLE); /**/ } int main(void) { unsigned char data=0; Uart_Int(); // while(1) { while (USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); USART_SendData( USART2, 'a'); } } what kind of problem it has.....?2015-05-11 4:27 AM
RCC_APB2PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE); // APB1 APB1 - Fix This
You can also lose the USART_Clock stuff, it doesn't do anything, isn't needed, and it is in the wrong spot.2015-06-20 4:17 AM
Thank you so much clive1, problem solved.
2015-06-20 4:48 AM
Dear Clive1, Now i am using STM32f0 discovery board,(stm32f051r), i want to transmitte and receive Uart1 data over DMA, if i used Circular mode then any character received through uart1 send continuously, and if i used normal mode then nothing happen. no data receive or transmite, here is my code.
#include ''main.h'' uint8_t AckBuffer [0x02] = {0x00, 0x00}; static void USART_Config(void); DMA_InitTypeDef DMA_InitStructure; int main(void) { USART_Config(); //---------------- DMA_DeInit(DMA1_Channel3); DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&USART1->RDR;//USARTx_TDR_ADDRESS;// DMA_InitStructure.DMA_BufferSize = (uint16_t)1; DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)AckBuffer; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_Init(DMA1_Channel3, &DMA_InitStructure); DMA_DeInit(DMA1_Channel2); DMA_InitStructure.DMA_PeripheralBaseAddr =(uint32_t)&USART1->TDR; //USARTx_TDR_ADDRESS;// DMA_InitStructure.DMA_BufferSize = (uint16_t)1; DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)AckBuffer; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralDST; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_Init(DMA1_Channel2, &DMA_InitStructure); USART_DMACmd(USART1, USART_DMAReq_Rx, ENABLE); USART_DMACmd(USART1, USART_DMAReq_Tx, ENABLE); DMA_Cmd(DMA1_Channel2, ENABLE); DMA_Cmd(DMA1_Channel3, ENABLE); USART_ClearFlag(USART1, USART_FLAG_TC); DMA_ClearFlag(DMA1_FLAG_GL2); DMA_ClearFlag(DMA1_FLAG_GL3); while (USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); USART_SendData( USART1, 'F'); //------------------ while (1) {} } static void USART_Config(void) { USART_InitTypeDef USART_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA | RCC_AHBPeriph_GPIOA, ENABLE); USARTx_APBPERIPHCLOCK(RCC_APB2Periph_USART1, ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE); GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_1); GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_1); GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_3; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_Init(GPIOA, &GPIO_InitStructure); USART_InitStructure.USART_BaudRate = 115200; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USARTx, &USART_InitStructure); DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable;//Enable; DMA_InitStructure.DMA_Mode =DMA_Mode_Circular; //DMA_Mode_Normal;// DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; USART_Cmd(USARTx, ENABLE); } #ifdef USE_FULL_ASSERT void assert_failed(uint8_t* file, uint32_t line) { /* Infinite loop */ while (1) { } } #endif2015-06-21 6:55 AM
2015-06-21 7:16 AM
Not sure I see the value of single byte DMA.
In normal mode you'd need to reconfigure the DMA after each byte is sent or received. I don't see any code managing that.2015-06-21 11:38 AM
2015-06-21 4:43 PM
Watch that you top post responses, and avoid using phone/tablet devices which don't' work well with this Microsoft ''forum'' software.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.