2014-03-17 7:12 PM
Hello,
I am planning on using the SDADC in STM32F37x microcontroller. The data sheets says the sampling frequency is between 500 kHz ~ 6 MHz, depending on the clock signal driving the SDADC. The output data rate is 4.167 ksps ~ 50 ksps accordingly. So it appears that the over sampling rate is 120. But the data sheet never says so. In between these two points, I can drive the SDADC with a clock signal derived from the system clock and get a output data rate of 1/120 of the frequency of the driving clock signal. Am I correct? Thanks for your input. Jim #stm32f373-sdadc2014-03-18 6:12 AM
The data sheet says the SDADC clock frequency is 0.5 to 6 MHz.
The output data sampling rate scales with clock frequency. Cheers, Hal2014-03-19 1:59 AM
Hi Jim,
Your analysis is correct: there is a fixed oversampling ratio 120 (input sampling frequency vs. output data rate). Input sampling frequency is the SDADC clock which you may set by software. -Mayla-Hello,
I am planning on using the SDADC in STM32F37x microcontroller. The data sheets says the sampling frequency is between 500 kHz ~ 6 MHz, depending on the clock signal driving the SDADC. The output data rate is 4.167 ksps ~ 50 ksps accordingly. So it appears that the over sampling rate is 120. But the data sheet never says so. In between these two points, I can drive the SDADC with a clock signal derived from the system clock and get a output data rate of 1/120 of the frequency of the driving clock signal. Am I correct? Thanks for your input. JimTo give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-05-07 3:59 AM
Is there some undocumented low-pass or filtering inside the SDADC?
Example: The SDADC is driven at 6MHz single channel 50ksmpls for two SDADC-units. This means every 20µs took one sample. The ADC's became now two signals: one pwm readback and one RC-lowpass answer. The rising edge of both signals are faster than 10µs. The ADC's now samples the signals as rising for 3 samples, this means 60µs. That is a major fault! How can i avoid this to get the real signal read?2015-05-25 2:11 AM
In the SDADC is used Sinc filter with order 3 and oversampling 120. Therefore the rising edge is 3 samples. For continuous mode we must count with those 3 samples ''spreading'' if is used FAST mode (FAST=1).
In continuous mode with FAST=0 is data rate Fsdadc/360.In continuous mode with FAST=1 is data rate Fsdadc/120 (but ''spreading'' of output data).We’re moving the ST Community to a new platform to give you a better and more reliable community experience.