2016-03-10 3:21 PM
Where do I find information about noise of DAC in STM32F373, for example
Output Noise Spectral Density ?2016-03-14 7:20 AM
Hi ismail.carpenter,
Your request is not so obvious, could you please provide some more details?-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-03-14 1:49 PM
Hello,
the DAC noise depends on the sampling rate and the bit resolution you’ve chosen. If you have 4096 steps to sample 3 V one would expect to get roughly 1 mV per step (~70 dB SNR) however depending on the setup you're using (e.g a disco board) it might get worse. I’ve seen some 20 mV PP noise with repetitive 100 mV peaks inside on the scope screen while the STM32F37x DAC was outputting a constant voltage. However as mentioned this depends on the current setting (e.g. also what kind of periphery is additionally activated). Sometimes it’s useful to consider a reconstruction filter. Depending whether the application is a highend one would also consider to use a synthesizer ic instead to reach higher performance.
2016-03-14 10:58 PM
> Depending whether the application is a highend one would also consider to use a synthesizer ic instead to reach higher performance.
I'd second this. Having analog units (DAC, ADC) on the same silicon as digital circuitry switching in the high-MHz-range is incompatible with the idea of ''high end''. ADCs and DACs on a microcontroller are always a compromise and a convenience. If you need maximal quality, use external units.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.