2016-10-30 1:09 AM
I'm using the 32F334C8 Pa4 dac1_out1 channel.However, buffer is not working. Here is my code,
void DAC_Config(void)
{ DAC_InitTypeDef DAC_InitStructure; /* Configure DAC1 OUT1 ******************************************************/ /* GPIO Periph clock enable */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); /* Configure PA4 (DAC1_OUT1) as analog */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure); /* DAC1 Periph clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_DAC1, ENABLE); /* DAC1 deinitialize */ DAC_DeInit(DAC1); /* Fill DAC InitStructure */ DAC_InitStructure.DAC_Trigger = DAC_Trigger_None; DAC_InitStructure.DAC_Buffer_Switch = DAC_BufferSwitch_Disable ; // DAC_BufferSwitch_Enable; DAC_InitStructure.DAC_WaveGeneration = DAC_WaveGeneration_None; DAC_InitStructure.DAC_LFSRUnmask_TriangleAmplitude = DAC_LFSRUnmask_Bit0; /* DAC Channel1 Init */ DAC_Init(DAC1, DAC_Channel_1, &DAC_InitStructure);// DAC_Init(DAC2, DAC_Channel_1, &DAC_InitStructure); /* Enable DAC Channel1 */ DAC_Cmd(DAC1, DAC_Channel_1, ENABLE); /* Set DAC Channel1 DHR register: DAC1_OUT */ // DAC_SetChannel1Data(DAC1, DAC_Align_12b_R, (uint16_t)CurrentSenseTab[0]); }I think i can't open the buffer because i always see voltage at PA4 out pin. In programming manual i found that:The DAC1 channel 1 comes with an output buffer that can be used to reduce the outputimpedance on DAC1_OUT1 output, and to drive external loads directly without having toadd an external operational amplifier.
I hope i'll solve that problem. Thanks #stm32f3342016-10-30 3:24 AM
>
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
Not AF, analog. JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.