2020-01-29 9:37 AM
Hello all,
i have a Problem on a STM32F30x as described in the question.
I can´t achieve to connect TIM16CH1 and TIM17CH1 to GPIOB 8 and 9. The goal is to get a PWM signal on these pins based on a compare match.
Both Timers are running. If i read the corresponding TIM16->CNT rest. TIM17->CNT register i can see both are counting up and restarting after a overflow occurred. But i´m not getting a signal on the pin PB8 and PB9.
Here is my code:
/**
* System clock is initalized
*/
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM16, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM17, ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource8, GPIO_AF_1);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource9, GPIO_AF_1);
GPIO_InitTypeDef GPIOB_pwm_init;
GPIOB_pwm_init.GPIO_Mode = GPIO_Mode_AF;
GPIOB_pwm_init.GPIO_OType = GPIO_OType_PP;
GPIOB_pwm_init.GPIO_Pin = (GPIO_Pin_8 | GPIO_Pin_9);
GPIOB_pwm_init.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIOB_pwm_init.GPIO_Speed = GPIO_Speed_Level_3;
GPIO_Init(GPIOB, &GPIOB_pwm_init);
TIM_DeInit(TIM16);
TIM16->CR1 |= (0x01 << 7);
TIM16->CCMR1 |= (0x04 << 4 ) | (0x01 << 3);
TIM16->CCER |= (0x01);
TIM16->PSC = 71;
TIM16->ARR = 4000;
TIM16->CCR1 = 2000;
TIM_Cmd(TIM16, ENABLE);
TIM_DeInit(TIM17);
TIM17->CR1 |= (0x01 << 7);
TIM17->CCMR1 |= (0x04 << 4 ) | (0x01 << 3);
TIM17->CCER |= (0x01);
TIM17->PSC = 71;
TIM17->ARR = 4000;
TIM17->CCR1 = 2000;
TIM_Cmd(TIM17, ENABLE); I have spend hours reading through the reference manual but no hints.
Help is welcome!
2020-01-29 10:10 AM
TIM16 and TIM17 have break functionality, where there is an additional Master Output Enable bit that must be set to get any output on the pins.
TIM16->BDTR |= TIM_BDTR_MOE;
TIM17->BDTR |= TIM_BDTR_MOE;
2020-01-29 11:38 AM
Also note that both PSC and ARR are programmed with N-1 for N states, ie 0 .. N-1
You perhaps want 0 .. 3999, with the center at 2000, ie 0..1999, 2000..3999
2020-01-29 3:03 PM
Thank you @berendi for the explanation and @clive1 for your hint.
I was able to solve the problem end the oscilloscope is showing a nice pwm signal now.
Thanks 8) :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.