2017-10-06 3:35 AM
Hello everybody,
I am still having problems with the STM32F303 bootloader.
Description
On 3 out of 6 boards, the USB does never get enumerated. The boards keep resetting randomly - the reset is software.
On 2/6 boards everything works reliably, while the other board works 'sometimes'.
The HSE ready bit in RCC_CR is 1, and it seems to stay that way (the HSE bypass bit in RCC_CR is 0 - can it be a problem with an external oscillator?).
I have no clues. What I have discovered is that only at times the FW tries to configure the USB - at times it skips it. At times the FW ends in a loop where it keeps resetting the watch dog, at times it ends in a loop where it reads pin status from GPIOA and GPIOD. Most of the times it simply reset.
I cannot find out what causes this reset - all the vectors bring to 0x1fffed10. And, by the way, stepping through asm code can be very tiring. ;)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.