2015-08-11 12:40 AM
Hello,
I'm using timer3 to generate an interrupt every 10ms (it saves one value everytime to a buffer). Everything works fine until I try to save buffer data to 1 page of flash. It happens of course inside the interrupt function after a buffer is fully wrtten. The saving into flash function works fine but the problem is that when the saving happens in an interrupt my μC is just catching a huge lag and even reset button can't help about it. variables and interrupt function in timer module: extern uint32_t DataPage[512]; // flash page buffer extern unsigned long TablicaStron[128]; //table of flash pages extern uint32_t dana; // data to be saved into buffer extern int DataIndex; // pointer to another place in page buffer extern int PageNumber; extern uint32_t Address; extern TIM_HandleTypeDef htim2; /* USER CODE END 0 */ /* External variables --------------------------------------------------------*/ extern TIM_HandleTypeDef htim3; void TIM3_IRQHandler(void) { /* USER CODE BEGIN TIM3_IRQn 0 */ /* USER CODE END TIM3_IRQn 0 */ HAL_TIM_IRQHandler(&htim3); /* USER CODE BEGIN TIM3_IRQn 1 */ dana = htim2.Instance->CNT; // current encoder value write1BrickFlash( DataIndex, dana); // saves one data into buffer DataIndex++; if(DataIndex==512) { WriteFlashPage(); EraseDataPage(); //clears the buffer IncreasePageNumber(PageNumber); DataIndex=0; } /* USER CODE END TIM3_IRQn 1 */ } my flash saving function situated in main.c file module looks like that: static FLASH_EraseInitTypeDef EraseInitStruct; //Variable used for Erase procedure void WriteFlashPage(){ HAL_FLASH_Unlock(); int index=0; __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP|FLASH_FLAG_PGERR|FLASH_FLAG_WRPERR|FLASH_FLAG_BSY); EraseInitStruct.TypeErase = TYPEERASE_PAGES; EraseInitStruct.PageAddress = TablicaStron[PageNumber]; EraseInitStruct.NbPages = (TablicaStron[PageNumber+1] - TablicaStron[PageNumber])/FLASH_PAGE_SIZE; if (HAL_FLASHEx_Erase(&EraseInitStruct, &PageError) != HAL_OK) { while (1) { HAL_GPIO_WritePin(GPIOE, GPIO_PIN_13, GPIO_PIN_SET); //Page erase error } } Address = TablicaStron[PageNumber]; while (Address < TablicaStron[PageNumber+1]) { if (HAL_FLASH_Program(TYPEPROGRAM_WORD, Address, DataPage[index]) == HAL_OK) { index++; Address = Address + 4; } } HAL_FLASH_Lock(); } I have no idea where the problem lies. Any help will be appreciated. Regards Dominik O.2015-08-11 2:09 AM
I also tried to call flash saving function inside the main loop after the timer fills the buffer, but each time the saving process occurs I can no longer start my timer (using button) because then the program is catching a lag.
Flash writing function works fine, I checked it (I programmed a button to write next flash page everytime it's pushed. After that I can see the correct data written in flash registers on exact pages I wanted. Timer alone also works fine by evoking an interrupt every 10ms. Sometimes a compiler is also giving such a result: Open On-Chip Debugger 0.9.0-dev-00415-g2d4ae3f-dirty (2015-04-22-11:10) Licensed under GNU GPL v2 For bug reports, read http://openocd.org/doc/doxygen/bugs.html Info : auto-selecting first available session transport ''hla_swd''. To override use 'transport select <transport>'. adapter speed: 1000 kHz adapter_nsrst_delay: 100 Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD none separate srst_only separate srst_nogate srst_open_drain connect_deassert_srst Info : Unable to match requested speed 1000 kHz, using 950 kHz Info : Unable to match requested speed 1000 kHz, using 950 kHz Info : clock speed 950 kHz Info : STLINK v2 JTAG v23 API v2 SWIM v0 VID 0x0483 PID 0x3748 Info : using stlink api v2 Info : Target voltage: 2.928257 Info : stm32f3x.cpu: hardware has 6 breakpoints, 4 watchpoints Info : accepting 'gdb' connection on tcp/3333 Info : device id = 0x10036422 Info : flash size = 256kbytes undefined debug reason 7 - target needs reset Info : Unable to match requested speed 1000 kHz, using 950 kHz Info : Unable to match requested speed 1000 kHz, using 950 kHz adapter speed: 950 kHz target state: halted target halted due to debug-request, current mode: Thread xPSR: 0x01000000 pc: 0x08005cd8 msp: 0x2000a000 Info : Unable to match requested speed 1000 kHz, using 950 kHz Info : Unable to match requested speed 1000 kHz, using 950 kHz adapter speed: 950 kHz target state: halted target halted due to debug-request, current mode: Thread xPSR: 0x01000000 pc: 0x08005cd8 msp: 0x2000a000 Info : Unable to match requested speed 8000 kHz, using 4000 kHz Info : Unable to match requested speed 8000 kHz, using 4000 kHz adapter speed: 4000 kHz target state: halted target halted due to breakpoint, current mode: Thread xPSR: 0x61000000 pc: 0x2000003a msp: 0x2000a000 Info : Unable to match requested speed 1000 kHz, using 950 kHz Info : Unable to match requested speed 1000 kHz, using 950 kHz adapter speed: 950 kHz target state: halted target halted due to debug-request, current mode: Thread xPSR: 0x01000000 pc: 0x08005d80 msp: 0x2000a000 Info : dropped 'gdb' connection2015-08-11 4:12 AM
Okey, I no longer have this problem with matching speed. I add to debug configuration startup these lines:
monitor reset monitor halt monitor flash protect 0 0 11 off but it still doesnt solve the problem of halting the program when trying to start a timer after writing to flash.2015-08-12 2:06 AM
I have moved timer IT function into main module using HAL_TIM_PeriodElapsedCallback() and it works fine until 3rd page of flash is written. Then it freezes. Either way if I first save data to flash and then start the timer if freezes instantly and I have to programm the Microcontroller again.
edited: I fount the problem. Timer is blocking the microcontroller after calling of HAL_FLASH_Unlock() HAL_FLASH_Lock(); But I dont know the reason of such a behaviour. Any help will be appreciated.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.