2014-01-16 7:09 AM
Firstable, sorry for so many new topics, but as i dig deeper and deeper into programming stm32 boards, i find a lot new questions. I wasn't able to find a topic which relates to my problem, so i just created a new, and here is my question: I know stm32f3 board has embedded comparators. Is it possible to put a ramp signal from external generator into one into I/O pins and the same signal into one of comparator's input. Then detect a falling edge of the signal go to interrupt which starts timer, and stops it when signal reaches threshold value? Is it possible to change treshold value in my program? Maybe there are some examples written by ST for comparators usage? Any help and answers to my this problem will be highly appreciated. Thanks in advance.
Edit: I found example on OPAMP_PGA for stm32, but that just gives me understanding how to configure comparator.2014-01-20 8:58 AM
NVIC_SystemReset(); // Perform a system reset. Dont know if this is needed.
That would be a NO! Perhaps you're thinking of SystemInit(), which depending on your tools chain is usually called by start up code prior to calling main(). It's part of the CMSIS design, ignored by CooCox I'd also move any clock enablement early in the configuration, the DeInit() routines likely expect the clocks to be enabled, I'm not convinced the peripheral Reset functions are asynchronous.2014-01-20 9:10 AM
Edit: Thank you for your help. Now my code is working and comparator work's as it should. I have a question though. If i look up no PF4 with scope, i see small voltage “jumps“ even without running my code. I also see that on some PA pins. Have u any idea why is that?
Thank you very much for your help again and answers.2014-01-20 11:43 AM
i see small voltage “jumps“
PF4 pin is digital logic. As long as it doesn't jump between logic level ''0'' and ''1'' levels, this is normal noise pickup. If you see the same problem on PA1 when the signal source is connected, then further investigation might be needed. Cheers, Hal2014-01-24 2:41 AM
Thank you for your help. I still didn't manage to do what i want. I want to use the EXTI interrupt to detect the falling edge of the signal connected to the I/O pin, then start a timer which would stop when comparator output goes to high level, however nothing works. My code now goes as follows:
#include
''main.h''
#include
''stdio.h''
TIM_ICInitTypeDef TIM_ICInitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
TIM_TimeBaseInitTypeDef TIM_TimeBaseInitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
EXTI_InitTypeDef EXTI_InitStructure;
COMP_InitTypeDef COMP_InitStructure;
void
EXTI1_IRQHandler(void
){
if
(EXTI_GetITStatus(EXTI_Line1) != RESET)//
Check
if
EXTI_Line1
is
asserted
{
GPIOE->ODR ^= GPIO_Pin_8;
}
EXTI_ClearITPendingBit(EXTI_Line1);
//
Clear
EXTI
LINE1
pending
bit
}
void
EXTI1_Config(void
){
SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOA, EXTI_PinSource1);
//
Connect
EXTI1
Line
to
PA1
pin
/*
Configure
EXTI1
line
*/
EXTI_InitStructure.EXTI_Line = EXTI_Line1;
//
Line1
EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;
//
Interrupt
mode
EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling;
//
Detect
falling
edge
of
the
external
signal
connected
to
PA1
EXTI_InitStructure.EXTI_LineCmd = ENABLE;
//
Enable
EXTI
line
EXTI_Init(&EXTI_InitStructure);
//
Send
parameters
to
the
registers
/*
Configure
NVIC
*/
NVIC_InitStructure.NVIC_IRQChannel = EXTI1_IRQn;
//
Select
NVIC
channel
to
be
configured
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority =
0x0F
;//
Set
priority
to
the
lowest
NVIC_InitStructure.NVIC_IRQChannelSubPriority =
0x0F
;//
Set
sub-priority
to
the
lowest
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
//
Enable
IRQ
channel
NVIC_Init(&NVIC_InitStructure);
//
Send
parameters
to
the
registers
}
void
Comparator_Config(void
){
/*
Configure
PA1
analog
mode:
It
is
used
as
Comparator1
analog
input
*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
//
Analog
mode
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/*
Configure
PF4
in
Alternate
Function
mode:
it
is
used
as
Comparator1
output
*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
//
Alternate
function
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOF, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOF, GPIO_PinSource4, GPIO_AF_2);
//
Connect
Port
A
pin
6
to
comparator
output
COMP_InitStructure.COMP_InvertingInput = COMP_InvertingInput_VREFINT;
COMP_InitStructure.COMP_NonInvertingInput = COMP_NonInvertingInput_IO1;
COMP_InitStructure.COMP_Output = COMP_Output_None;
COMP_InitStructure.COMP_BlankingSrce = COMP_BlankingSrce_None;
COMP_InitStructure.COMP_OutputPol = COMP_OutputPol_NonInverted;
COMP_InitStructure.COMP_Hysteresis = COMP_Hysteresis_No;
//
Do
not
use
Hysteresis
COMP_InitStructure.COMP_Mode = COMP_Mode_UltraLowPower;
//
Ultra
low
power
mode
COMP_Init(COMP_Selection_COMP1, &COMP_InitStructure);
//
Enable
COMP
parameters
COMP_Cmd(COMP_Selection_COMP1, ENABLE);
//
Enable
comparator1
}
int
main(void
){
RCC->AHBENR |=
1
<<21
;//
Enable
clock
for
port
E
RCC->APB1ENR |=
1
<<1
;//
enable
clock
for
Timer3
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);
//
Timer2
clock
on
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
//
GPIOA
clock
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOF, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);
//
Enable
the
SYSCFG
APB
clock
to
get
write
access
to
comparator
register
and
EXTI
line
interrupts
COMP_DeInit(COMP_Selection_COMP1);
//
Reset
comp1
parameteres
to
default
values
//
Port
E
pin
8
(blue
LED)
configuration
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOE, &GPIO_InitStructure);
EXTI1_Config();
EXTI1_IRQHandler();
//
Comparator_Config();
//
Uncomment
this
line
and
comparator
works,
but
the
code
never
jumps
to
EXTI1_IRQHandler.
Comment
this
line
and
then
code
goes
to
EXTI1_IRQHandler
while
(1
){
//
Do
nothing
}
}
As i stated in the code, uncommenting the line Comparator_Config() in the main function get's comparator to work, but then code never jumps to EXTI line IRQ handler. If i comment that line, comparator obviously doesn't work, but then my code is able to jump to EXTI_IRQHandler. Could anyone explain why this behaviour is caused? Is it because EXTI Line 1 uses the same pin as Comparator input? OR is it because that it requires GPIO pins to be configured in input mode if i want to use EXTI interrupt, but i already have configured the pin in analog mode for Comparator? Or i have completely wrong understanding of how EXTI interrupts work? I'll appreciate any help for solving this problem. Thanks in advance.2014-01-24 1:21 PM
You seem to have taken a step backwards. After setting up your comparator falling edge detect criteria and connecting the comparator output to PF4, you then connect the EXT interrupt to PA1, bypassing the comparator output.
My guess is that you are confused over the edge detector logic in the EXT ciruitry. As I stated before, this is a digital logic edge criteria, your sine wave input is an analog signal, so you need to use the setup you have in place for the comparator inputs as your edge detector. See Section 11.2.6 in the F3 reference manual. The table there identifies EXTI4 as the interrupt connected to PF4, and that should then be the handler that starts the timer going. After you get the timer going correctly, then you need to set up another comparator with low level detection connected to another EXT interrupt to stop the timer when the low level criteria is met. Cheers, Hal2014-01-24 2:32 PM
From your post i now see that i misunderstood the EXTI interrupt and edge detecting criteria. Thanks a lot for your help and time. I'll try to do this now and give you a feedback.
Cheers, Arganas.2014-01-28 5:12 AM
I just wanted to give you a feedback. Thank you for your help, time and comments. It helped me a lot and i managed to do what i want.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.