2014-01-29 5:50 AM
I`m trying to configure a STM32F3 Project with the CoIDE 1.7.6 to run an ISR from CCM RAM basing on the AN4296 application note, but I can't put it to work with the CoIDE.
2014-01-29 7:56 AM
in 1.7.5:
C file:#define CCMRAMFUNC __attribute__ ((long_call, section (''.ccmramtext'')))and add to function declarations you want to execute in CCM.in your .ld file:MEMORY{ rom (rx) : ORIGIN = 0x08000000, LENGTH = 0x00040000 ram (rwx) : ORIGIN = 0x20000000, LENGTH = 0x0000a000 ram1 (rwx) : ORIGIN = 0x10000000, LENGTH = 0x00002000}between .data and .bss sections put: _siccmramtext = ADDR(.text) + SIZEOF ( .text ) + SIZEOF ( .data ); .ccmramtext : AT (_siccmramtext) { _sccmramtext = .; *(.ccmramtext .ccmramtext.*) . = ALIGN(4); _eccmramtext = . ; } > ram1and to your startup file put this after data segment initialization, just before bss zeroing pulSrc = &_siccmramtext; for(pulDest = &_sccmramtext; pulDest < &_eccmramtext; ) { *(pulDest++) = *(pulSrc++); }hope it helps,karel
2014-01-30 1:36 PM
Karel,
Thanks very much. It solved my problem. Ari.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.