2015-08-03 4:35 AM
Hi,
I am using STM32f3 ARM cotex3. I am working on Firmware Upgrade where one of my code executes from 0x08000000 and other i am locating my 2nd application at 0x08010000 . I have used two method one with the scatter file where i changed IROM1 address to 0x08010000 and kept offset vector 0x10000 but problem is my program is not executing from the 0x08010000 location.2. Other , through the UART i am wring to the location 0x08010000 while i am able to write the code but unable to jump 0x08010000 th loaction . my jump code : JumpAddress = *(__IO uint32_t*) (0x08010000 + 4); Jump_To_Application = (pFunction) JumpAddress; /* Initialize user application's Stack Pointer */ __set_MSP(*(__IO uint32_t*) 0x08010000 ); Jump_To_Application(); if any one has idea then please help me ?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.