2019-08-13 1:52 AM
Hi.
yesterday, my stm32 board run was good.
today, I add to code(printf...). but my board is hangup.
I was check memory over. but, i use 25%.
project.map
177 901 bytes of readonly code memory
54 396 bytes of readonly data memory
87 330 bytes of readwrite data memory
Errors: none
Warnings: none
Internal memory of STM32F207 is 0x08000000~0x080fffff.
I was only add the "printf" code. but, my board is hangup.
I was debugging. i was find the hangup position the GPIO Initial.
assert_param(IS_GPIO_OTYPE(GPIO_InitStruct->GPIO_OType));
I don't know. problem at the this position.
yesterday, GPIO initial code is good.
I don't know, that I add only some code. and I have this problem?
thank you
Solved! Go to Solution.
2019-08-13 9:20 PM
Thank you.
I was solved the problem.
I was change thes position of GPIO Initial().
and then, this problem is clean.
2019-08-13 7:54 AM
Perhaps use a debugger and determine where it HangUp? ie press STOP and see.
Check for NUL pointers and incomplete structure initialization. Be aware of how local/auto variables allocate from dirty stack memory.
If it asserts because of particular fields, perhaps check those.
Make sure you have sufficient stack.
Be able to determine if it gets stuck in the HardFault_Handler() or Error_Handler()
Make sure you have libraries and suitable targeting of putchar() type routines for printf() to utilize, ie targeting an initialized USART or SWV debug channel.
2019-08-13 9:20 PM
Thank you.
I was solved the problem.
I was change thes position of GPIO Initial().
and then, this problem is clean.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.