2016-08-30 12:43 AM
based on stm32cubemx with library 1.4.0 for stm32f205
with interrupt receiving the fifonumber within the structCanRxMsgTypeDef
is not set by the functionCAN_Receive_IT()
instm32f2xx_hal_can.c
if the user/application does not care about the fifo it makes no big deal.patch for stm32f2xx_hal_can.c* @version V1.1.3
* @date 29-June-2016add following in stm32f2xx_hal_can.c @ line #1346hcan->pRxMsg->FIFONumber = FIFONumber;
2016-09-01 6:31 AM
Hi d-chris,
Yes you are right. This already reported in this [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Configure%20CAN%20to%20receive%20in%20both%20FIFOs&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=53]thread. I report it to be fixed.-Hannibal-2016-12-06 8:43 PM
FTITI.Walid
:Great, thanks. I was just about to report this again for the F2 series.
I reported the same issue for the F3 library a while ago and thought it would be fixed by now.
https://community.st.com/0D50X00009XkeqISAR
Can you please make sure this gets fixed for all mcu series?
Thanks!
2016-12-06 11:04 PM
There seem to be a crate load of these DEAD LINK markers, how should we go about fixing and identifying these?
2016-12-07 1:53 AM
Hi Clive,
This deak link issue in the new platform is reported and it is under investigation.
-Walid F-
2016-12-07 4:19 AM
Hi
Roehrig.Valentin
,I confirm that the same issue exist in this 1.4.0 Cube version/ 1.1.3 driver version. I report it to be fixed in the next version .
Thanks for the contribution.
-Walid F-
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.