2025-09-22 11:49 PM
Hey guys!
I am currently working on stm32F2 series, the issue i was facing in HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) when the UART transmit the first byte the interrupt call back function is not called instead calling the RxCpltCallback it call the " USART1_IRQHandler(void) "and the RxCpltCallback function does not trigger at first byte in UART at the second byte it call the RxCpltCallback function and it works fine and i attached the code i was wrote
#include "main.h"
UART_HandleTypeDef huart1;
UART_HandleTypeDef huart3;
unsigned char ra_buffer[32];
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART1_UART_Init(void);
static void MX_USART3_UART_Init(void);
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_USART1_UART_Init();
MX_USART3_UART_Init();
HAL_UART_Receive_IT(&huart1,ra_buffer,12);
while (1)
{
HAL_Delay(1000);
}
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
HAL_UART_Receive_IT(&huart1,ra_buffer,1);
HAL_UART_Transmit(&huart3,ra_buffer, 1,100);
}
2025-09-23 12:16 AM
> HAL_UART_Receive_IT(&huart1,ra_buffer,12);
will call HAL_UART_RxCpltCallback only after 12 bytes received.
USART1_IRQHandler is called internally after each byte until the limit you have set (here: 12) ist reached.
2025-09-23 1:58 AM
Hi @Ravi_shankar ,
Your issue is that the first byte received on UART1 does not trigger the HAL_UART_RxCpltCallback immediately, but the second byte does. This behavior usually happens because of how the UART receive interrupt and buffer size are configured and how the callback is re-armed.
Your initial call is:
This means the HAL driver waits to receive 12 bytes before triggering the HAL_UART_RxCpltCallback. So the callback will not be called after the first byte, but only after 12 bytes are received.
In the Callback:

Here you re-arm the receive interrupt to receive only 1 byte at a time. This is why after the first 12 bytes, the callback is triggered, and then subsequent single bytes trigger the callback immediately.
If you want to receive one byte at a time and have the callback called immediately after each byte, you should:

Best Regards,
Aime
2025-09-25 1:43 AM
Hello @Ravi_shankar
Please any update on this thread?
2025-10-23 11:44 PM
it is good explanation of other replies for how the 'HAL_UART_RxCpltCallback' work, but generally, we don't put any functions in HAL_UART_RxCpltCallback() but just trigger a flag to indicate one RX completely, because IT handler must be process short code and return quickly to avoid conflict with other IT coming. just like
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
UART_RX_ready = 1;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.