2012-09-21 11:25 AM
Hi All,
I am seeking help on why I2C2 bus is not communicating. I can see a start condition and then CLK is held low while DATA is held high. Any guidance would be appreciated. Thanks. &sharpinclude ''oneWire.h''&sharpinclude ''stm32f10x_lib.h''&sharpinclude ''stm32f10x_i2c.h''&sharpinclude ''stm32f10x_rcc.h''void DS2482_Init(void){ GPIO_InitTypeDef GPIO_InitStructure; I2C_InitTypeDef I2C_InitStructure; I2C_DeInit(DS2482_I2C); /* Enable peripheral clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C2, ENABLE); /* Enable GPIOB clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE); /* Enable AFIO clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE); /* Configure I2C2_SCL and I2C2_SDA */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_OD; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOB, &GPIO_InitStructure); /* DS2483 peripheral configuration */ I2C_InitStructure.I2C_Mode = I2C_Mode_I2C; I2C_InitStructure.I2C_DutyCycle = I2C_DUTYCYCLE; I2C_InitStructure.I2C_OwnAddress1 = DS2482_I2C_ADDRESS; I2C_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_InitStructure.I2C_ClockSpeed = DS2482_I2C_SPEED; /* enable the I2C peripheral */ I2C_Cmd(DS2482_I2C, ENABLE); I2C_Init(DS2482_I2C, &I2C_InitStructure); }int DS2482_channel_select(int channel){ // select the 1-wire channel on DS2482-800 // Returns: TRUE if channel selected // FALSE if device not detected unsigned char ch, ch_read, check; /* while the bus is busy */ while(I2C_GetFlagStatus(DS2482_I2C, I2C_FLAG_BUSY)); I2C_GenerateSTART(DS2482_I2C, ENABLE); while(!I2C_CheckEvent(DS2482_I2C, I2C_EVENT_MASTER_MODE_SELECT)); I2C_AcknowledgeConfig(DS2482_I2C, ENABLE); //I2C_Send7bitAddress(DS2482_I2C, DS2482_I2C_ADDRESS, I2C_Direction_Transmitter); I2C_Send7bitAddress(DS2482_I2C, 0x30, I2C_Direction_Transmitter); while(!I2C_CheckEvent(DS2482_I2C, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); I2C_SendData(DS2482_I2C, DS2482_CHSL); switch (channel) { default: case 0: ch = 0xF0; ch_read = 0xB8; break; case 1: ch = 0xE1; ch_read = 0xB1; break; case 2: ch = 0xD2; ch_read = 0xAA; break; case 3: ch = 0xC3; ch_read = 0xA3; break; case 4: ch = 0xD4; ch_read = 0x9C; break; case 5: ch = 0xE5; ch_read = 0x95; break; case 6: ch = 0x96; ch_read = 0x8E; break; case 7: ch = 0x87; ch_read = 0x87; break; }; I2C_SendData(DS2482_I2C, ch); // send START condition a second time I2C_GenerateSTART(DS2482_I2C, ENABLE); // send DS2482 address for read I2C_Send7bitAddress(DS2482_I2C, DS2482_I2C_ADDRESS, I2C_Direction_Receiver); check = I2C_ReceiveData(DS2482_I2C); // send STOP condition I2C_GenerateSTOP(DS2482_I2C, ENABLE); return (check == ch_read);} #stm32f10x2012-11-29 11:45 AM
Hopefully you've resolved this by now, but this might help the next person to come along. I ran into a similar problem on my STM32F100C8, and I narrowed it down to the AFIO being enabled. What I had to do was enable the AFIO, do my remapping, then disable the AFIO periphery. Then I set up the I2C and it works fine, and it appears the remapping persists. I don't have a lot of experience on this yet, but it looks to be a viable solution.
Question is, why does enabling the AFIO periphery mess with I2C? I tried to disable the remap of the I2C, thinking it somehow remapped it automatically, but that didn't seem to be the case. Nothing in the documentation jumped out at me.2012-11-29 12:10 PM
You have to enable the AFIO clock to do the remapping because that's where the mapping register/latches are situated, are you saying the AFIO clock must then be disabled before the I2C will work?
The OP isn't remapping the pins.2012-11-29 12:51 PM
That is correct. The actual remapping call did not affect I2C, but enabling the AFIO peripheral did. (I wasn't remapping anything for the I2C, but disabling JTAG as we use 2-wire SWD only and needed to repurpose the JTAG lines. This came up as a side-effect).
As a side note, the AFIO doesn't show up as a peripheral in the block diagram or clock tree in the RM, so it took me a little while to figure out it needed to be enabled before the remap command would be effective.2012-12-03 8:45 AM
Update:
That's apparently only during I2C initialization. After the I2C is up, I added some more code and enable the AFIO again, and this time I leave it enabled and everything is working. Again, this is the STM32F100C8T6B. I don't see an obvious date code on the chip.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.