2012-06-17 10:40 PM
HI I want to use DMA to Recieving data via uart (rs485)
I want to use 20byte buffer but for siplicity in this exaple is shown only 1byte buffer... int main(void){ RCC_Configuration(); GPIO_Configuration(); USART_Configuration(); DMA_Configuration(); NVIC_Configuration_DMA_RX(); while(1){ }; } /******************************************************************************/ void RCC_Configuration(void) { /* Enable DMA clock */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE); /* Enable GPIO bank clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE); /* Enable UART clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); } /******************************************************************************/ void GPIO_Configuration(void) { GPIO_InitTypeDef GPIO_InitStructure; /* Configure USART Tx as alternate function push-pull */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; // PA.09 USART1.TX GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Configure USART Rx as input floating */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; // PA.10 USART1.RX GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &GPIO_InitStructure); } /******************************************************************************/ void USART_Configuration(void) { USART_InitTypeDef USART_InitStructure; /* USART resources configuration (Clock, GPIO pins and USART registers) ----*/ /* USART configured as follow: - BaudRate = 115200 baud - Word Length = 8 Bits - One Stop Bit - No parity - Hardware flow control disabled (RTS and CTS signals) - Receive and transmit enabled */ USART_InitStructure.USART_BaudRate = 115200; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_RTS; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; /* USART configuration */ USART_Init(USART1, &USART_InitStructure); /* Enable the USART1 */ USART_Cmd(USART1, ENABLE); USART_ITConfig(USART1, USART_IT_RXNE, ENABLE); /* Enable DMA Requests*/ USART_DMACmd(USART1, USART_DMAReq_Rx, ENABLE); USART_DMACmd(USART1, USART_DMAReq_Tx, ENABLE); } /******************************************************************************/ /** * @Brief * @Parameter None * * @Return None */ void DMA_Configuration(void) { // USART1 Channel 4, USART2 Channel 7, USART3 Channel 2 /***TX********************/ DMA_DeInit(DMA1_Channel4); DMA_Cmd(DMA1_Channel4, DISABLE); /***RX********************/ DMA_DeInit(DMA1_Channel5); DMA_Cmd(DMA1_Channel5, DISABLE); } /******************************************************************************/ void DMA_USART_Rx (void){ DMA_InitTypeDef DMA_InitStructure; DMA_DeInit(DMA1_Channel5); DMA_InitStructure.DMA_PeripheralBaseAddr = (u32)&USART1->DR; DMA_InitStructure.DMA_MemoryBaseAddr = (u32)RXpacket; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC; DMA_InitStructure.DMA_BufferSize = 1; //20 in the end DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte; DMA_InitStructure.DMA_Mode = DMA_Mode_Normal; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_ITConfig(DMA1_Channel5,DMA_IT_TC,ENABLE); DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; DMA_ClearFlag(DMA1_FLAG_TC5); DMA_Init(DMA1_Channel5, &DMA_InitStructure); DMA_Cmd(DMA1_Channel5, ENABLE); /* Wait of DMA completion */ USART_Cmd(USART2, ENABLE); DMA_ITConfig(DMA1_Channel5, DMA_IT_TC , ENABLE); while(DMA_GetFlagStatus(DMA1_FLAG_TC5) == RESET); /* Loop until the end of transmit */ while(USART_GetFlagStatus(USART1, USART_FLAG_TC) == RESET); } /******************************************************************************/ void NVIC_Configuration_DMA_RX(void) { NVIC_InitTypeDef NVIC_InitStructure; //Enable the USARRx Interrupt NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel5_IRQn ; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;//ENABLE NVIC_Init(&NVIC_InitStructure); /******************************************************************************/ void DMA1_Channel5_IRQHandler(void) { /*This part never start*/ } /******************************************************************************/ BUT WHEN I USED : /******************************************************************************/ void NVIC_Configuration_Irq(void) { NVIC_InitTypeDef NVIC_InitStructure; //Enable the USART_Rx Interrupt NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;//ENABLE NVIC_Init(&NVIC_InitStructure); } /******************************************************************************/ void USART1_IRQHandler(void) //Reading data { GPIO_WriteBit(LED_PORT, GPIO_Pin_13, Bit_SET); if ((USART1->SR & USART_FLAG_RXNE) != (u16)RESET); DMA_USART_Rx(); } /******************************************************************************/ iTS FIRST TIME GO IN USART1 INTERUPT AND THEN IN DMA1_Channel5.... sorry about your time but i cant find some DMA Rx example ..... second problem is that i want to use 20byte buffer - but in debugger always i recieve only firt i use -DMA_InitStructure.DMA_BufferSize = 20; and in debugger i see that first is recieved bud only firt isnt problem that dma cant read whole buffer -its read one by one ? somewhere i read that the DMA_IT_TC is possible to use only in M2M mode .... would you be so kind and take a look at code thanks2012-06-18 6:38 AM
Suggest to download STM32F2xx Standard Peripheral Library example ?For USART, there is an example of 2 boards communication.
(\USART\USART_TwoBoards\DataExchangeDMA) The readme.txt says ''In both boards, the data transfers is managed using the USART Tx/Rx channels DMA requests.'' hope it helps2012-06-25 11:50 PM
thanks i ll check it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.