2020-09-23 7:14 AM
I'm trying to use the standby mode of STM32F and waking it up by WKUP (PA0) pin.
Going to standby seems OK, power consumption goes to 4 uA.
If I reset MCU with RESET pin, it starts normally: after 250 ms delay it goes to sleep and consumes 4 uA
https://i.stack.imgur.com/nDM6f.png
But if I wake it up with WKUP pin it behaves strangely: consumption stays on a "run" level and I see cycles off my 250 delay, MCU keeps restarting instead of going to sleep.
https://i.stack.imgur.com/KYPqM.png
My code is really simple:
#include <stm32f1xx_hal.h>
#ifdef __cplusplus
extern "C"
#endif
void SysTick_Handler(void)
{
HAL_IncTick();
HAL_SYSTICK_IRQHandler();
}
void Error_Handler()
{
__asm("bkpt 255");
__asm("bx lr");
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = { 0 };
RCC_ClkInitTypeDef RCC_ClkInitStruct = { 0 };
__HAL_RCC_AFIO_CLK_ENABLE();
__HAL_RCC_PWR_CLK_ENABLE();
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI | RCC_OSCILLATORTYPE_LSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.LSIState = RCC_LSI_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.PLL2.PLL2State = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK
| RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
/** Configure the Systick interrupt time
*/
__HAL_RCC_PLLI2S_ENABLE();
}
int main(void)
{
HAL_Init();
SystemClock_Config();
__HAL_AFIO_REMAP_SWJ_NOJTAG();
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
HAL_Delay(250);
HAL_PWR_EnterSTANDBYMode();
}
Solved! Go to Solution.
2020-09-23 7:38 AM
Found a solution in errata sheet and with a help of the internet:
int main(void)
{
HAL_Init();
SystemClock_Config();
__HAL_AFIO_REMAP_SWJ_NOJTAG();
HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN1);
PWR->CR |= PWR_CR_CWUF;
if (__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET) {
/* System resumed from STANDBY mode */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
/* Clear StandBy flag */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
/* Clear Wakeup flag */
}
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
HAL_Delay(250);
HAL_PWR_EnterSTANDBYMode();
}
2020-09-23 7:38 AM
Found a solution in errata sheet and with a help of the internet:
int main(void)
{
HAL_Init();
SystemClock_Config();
__HAL_AFIO_REMAP_SWJ_NOJTAG();
HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN1);
PWR->CR |= PWR_CR_CWUF;
if (__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET) {
/* System resumed from STANDBY mode */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
/* Clear StandBy flag */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
/* Clear Wakeup flag */
}
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
HAL_Delay(250);
HAL_PWR_EnterSTANDBYMode();
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.