2014-12-15 4:50 AM
Gentlem,
my question: The STMFlashDemonstrator 2.7.0 after loading a program in to the STM32F103ZET6, while verifying, brings the error: ''...The page may be write protected. Please disable the write protection...''. It's not possible because I have checked (with Rowley debugger) the OptionBytes WRP, they are all 0xFF. And the RDP is 0xA5. And the Rowley debugger loads the program at the mentioned page whitout error. How can it be, do you have an idea ?2014-12-15 11:45 AM
A communication problem? A low quality USB-to-Serial dongle, perhaps using one of Prolific's current or older broken drivers?
The boot loader is pretty fragile once it's auto-bauded the connection, and they aren't many avenues to retry things.2014-12-16 3:59 AM
It's curios the verifying error appears not for all STM32F103ZET6.
Thanks for your reply Clive! I will try your suggestions.2014-12-18 3:43 AM
I tried other STM32F103ZET6 too and also with another USB cable to the dongle.
The verifying error doesn't appears with STMFlashloader 2.5.0 for all STM32F103ZET6. But therefor with STMFlashloader 2.7.0. Yes it's funny, anyway. Thanks for your reply!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.