2014-07-11 6:32 PM
hi everyone,
how can I use the SPI3 DMA TX,the following is my configuration(it do not work):RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE);//IO?? RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA2, ENABLE);//DMA 2???? //RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE); /* ??SPI3?? */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI3, ENABLE); /* SPI3?? */ SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_CPOL = SPI_CPOL_High; SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitStructure.SPI_CRCPolynomial = 7; SPI_Init(SPI3, &SPI_InitStructure); SPI_I2S_DMACmd(SPI3, SPI_I2S_DMAReq_Tx, ENABLE); /* ??SPI1 */ SPI_Cmd(SPI3, ENABLE); DMA_DeInit(DMA2_Channel2); DMA_InitStructure.DMA_PeripheralBaseAddr = SPI3->DR; DMA_InitStructure.DMA_MemoryBaseAddr = (u32)leddis18; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralDST; DMA_InitStructure.DMA_BufferSize = 100; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte; DMA_InitStructure.DMA_Mode = DMA_Mode_Normal; DMA_InitStructure.DMA_Priority = DMA_Priority_VeryHigh; DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; DMA_Init(DMA2_Channel2, &DMA_InitStructure); #stm32-spi-dma2014-07-11 6:55 PM
It's an address, not the content of the register.
DMA_InitStructure.DMA_PeripheralBaseAddr = &SPI3->DR;We’re moving the ST Community to a new platform to give you a better and more reliable community experience.