2024-06-29 7:41 PM
no osc no resist no osc but it run and download with swd light led pb12 ,but when fixed pin anybody know
v2.9.0
-------------------------------------------------------------------
ST-LINK SN : 16004A002933353739303541
ST-LINK FW : V2J38S7
Board : --
Voltage : 3.17V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x414
Revision ID : Rev X
Device name : STM32F101/F103 High-density
Flash size : 512 KBytes
Device type : MCU
Device CPU : Cortex-M3
BL Version : --
Memory Programming ...
Opening and parsing file: BlinkSTM32FC8.ino.bin
File : BlinkSTM32FC8.ino.bin
Size : 12944 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 6]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:00.774
RUNNING Program ...
Address: : 0x8000000
Application is running, Please Hold on...
Start operation achieved successfullySolved! Go to Solution.
2024-06-30 5:59 AM
Dear @st128 ,
Welcome in STCommunity ! and glad to see it is working and so robust - However at real application you should follow minimum Hardware and passive components as this Application Note
Getting started with STM32F10xxx hardware development - undefined
Hope it helps you.
STOne-32.
2024-06-30 5:59 AM
Dear @st128 ,
Welcome in STCommunity ! and glad to see it is working and so robust - However at real application you should follow minimum Hardware and passive components as this Application Note
Getting started with STM32F10xxx hardware development - undefined
Hope it helps you.
STOne-32.
2024-07-01 3:10 AM
o,thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.