2017-04-25 10:49 AM
Dear Sir .
I am configuring A8,A9,A10,A11 for PWM OUTPUT.
I don't get an pwm output on PA9 ,
If I configure PA9 as output , Than I can toggle it.
Attached some code
/* Configure PWM Outputs */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStructure);// Enable TIM1 clock
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE);// Time Base configuration
TIM_TimeBaseStructure.TIM_Prescaler = 0x0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseStructure.TIM_Period = 0x3FF; // 10 bit TIM_TimeBaseStructure.TIM_ClockDivision = 0x0; TIM_TimeBaseStructure.TIM_RepetitionCounter = 0x0; TIM_TimeBaseInit(TIM1 , &TIM_TimeBaseStructure); // Channel 1,2 Configuration in PWM mode TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Enable; TIM_OCInitStructure.TIM_Pulse = 0x3ff; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low; TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCNPolarity_Low; TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Set; TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCIdleState_Reset; TIM_OC1Init(TIM1,&TIM_OCInitStructure); TIM_OCInitStructure.TIM_Pulse = 0x100; TIM_OC2Init(TIM1,&TIM_OCInitStructure); TIM_OCInitStructure.TIM_Pulse = 0x200; TIM_OC3Init(TIM1,&TIM_OCInitStructure); TIM_OCInitStructure.TIM_Pulse = 0x2ff; TIM_OC4Init(TIM1,&TIM_OCInitStructure); // TIM1 counter enable TIM_Cmd(TIM1,ENABLE); // Main Output Enable TIM_CtrlPWMOutputs(TIM1,ENABLE);Please Advise
2017-04-25 7:18 PM
Remap UASRT1 off these pins
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.