2019-05-21 5:34 AM
Hi All
I am trying to store variable in custom section withn FLASH.
In ld file I have the following
.flash_crc (LENGTH(FLASH) + ORIGIN(FLASH) - 1K):
{
. = ALIGN(4);
*(.flash_crc)
*(.flash_crc.*)
. = ALIGN(4);
} >FLASH = 0x00
Which (I believe) creates custom section at the last 1K page of 64K FLASH.
Then I am trying to declare a variable in my main.cpp
volatile uint32_t __attribute__((section(".flash_crc"), used)) __flash_crc;The map file gives me correct section location at 0x800fc00 and variabke fits inicely inside
.flash_crc 0x000000000800fc00 0x4
0x000000000800fc00 . = ALIGN (0x4)
*(.flash_crc)
.flash_crc 0x000000000800fc00 0x4 ./src/main.o
0x000000000800fc00 __flash_crc
*(.flash_crc.*)
0x000000000800fc04 . = ALIGN (0x4)In the code I am trying just to erase the FLASH page where the variable is located
FLASH_PrefetchBufferCmd( FLASH_PrefetchBuffer_Enable);
FLASH_SetLatency( FLASH_Latency_0);
FLASH_Status flashStatus;
FLASH_Unlock();
flashStatus = FLASH_ErasePage((uint32_t)0x800fc00);
FLASH_Lock();flashStatus is set to FLASH_COMPLETE, so I would expect everything is fine, and location 0x800fc00 is filled with 0xff.
In reality this does not happen, and contents of 0x800fc00 stays untouched after ERASE.
Strange enough, if I comment out variable declaration, then everything works fine and 0x800fc00 gets filled with 0xff after ERASE.
The same happens when I am trying to write something to 0x800fc00 using
FLASH_ProgramWord(0x800fc00, 0x12345678)With variable declared inside .flash_crc section nothing is written, when variable commnted out write succesfully occures.
Any help appreciated, thanks in advance
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.