2016-02-03 9:05 PM
I am using a minimal develpment board based on STM32F103C8. The board has an external crystal of 8Mhz.
I am trying to use PLL as my clock source (with input from HSE 8Mhz) upon boot but facing the following 2 issues: 1. When I use PLL multiplier as 9, the clock does not get generated at all. 2. When I use PLL multiplier as 8, the clock does get generated. SYSCLK is 64Mhz,however my HCLK is half of SYSCLK even though I am configuring it to be the same as SYSCLK
Below is my code (using PLL multiplier 8)
#include ''stm32f10x.h''
#include ''delay.h''
void
setupClock(
void
);
void
setupPins(
void
);
int
main(
void
)
{
RCC_ClocksTypeDef clock;
setupClock();
setupPins();
RCC_GetClocksFreq(&clock);
/*if(clock.HCLK_Frequency==64000000)
{
GPIO_SetBits(GPIOA, GPIO_Pin_6);
}*/
if
(RCC_GetSYSCLKSource() == 0x08 && clock.SYSCLK_Frequency == 64000000 && clock.HCLK_Frequency==32000000)
{
GPIO_SetBits(GPIOA, GPIO_Pin_6);
}
while
(1)
{
/*GPIO_SetBits(GPIOA, GPIO_Pin_6);
Delay_Ms(1000);
GPIO_ResetBits(GPIOA, GPIO_Pin_6);
Delay_Ms(1000);*/
}
}
void
setupClock(
void
)
{
ErrorStatus result;
RCC_DeInit();
RCC_HSEConfig(RCC_HSE_ON);
result = RCC_WaitForHSEStartUp();
if
(result==SUCCESS)
{
FLASH_PrefetchBufferCmd(ENABLE);
FLASH_SetLatency(FLASH_Latency_2);
//PLLCLK = (8Mhz * 9 = 72Mhz
RCC_PLLConfig(RCC_PLLSource_HSE_Div1,RCC_PLLMul_8);
RCC_PLLCmd(ENABLE);
//wait till PLL ready
while
(RCC_GetFlagStatus(RCC_FLAG_PLLRDY)==RESET)
{
}
//set PLL as SYSCLK source
RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);
//wait to verify pll is being used aS SYSCLK source
while
(RCC_GetSYSCLKSource() != 0x08)
{
}
//RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);
//setupPins();
//GPIO_SetBits(GPIOA, GPIO_Pin_6);
RCC_HCLKConfig(RCC_SYSCLK_Div1);
RCC_PCLK1Config(RCC_SYSCLK_Div2);
RCC_PCLK2Config(RCC_SYSCLK_Div1);
SystemCoreClockUpdate();
}
else
{
}
//enable clock to GPIOA
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);
}
void
setupPins(
void
)
{
GPIO_InitTypeDef gpio;
//set A6 as output
gpio.GPIO_Mode = GPIO_Mode_Out_PP;
gpio.GPIO_Pin = GPIO_Pin_6;
gpio.GPIO_Speed = GPIO_Speed_2MHz;
GPIO_Init(GPIOA, &gpio);
}
When I run the code, the led connected to PORT A6 lights up.
Please help. This is driving me nuts. I have checked it over and over again but can't find any issues
2016-02-03 10:07 PM
Dear Ankit,
Please verify the following point in your code-- 1. In file stm32f10x.h select right device
#if !defined (STM32F10X_LD) && !defined (STM32F10X_LD_VL) && !defined (STM32F10X_MD) && !defined (STM32F10X_MD_VL) && !defined (STM32F10X_HD) && !defined (STM32F10X_HD_VL) && !defined (STM32F10X_XL) && !defined (STM32F10X_CL)
/* #define STM32F10X_LD */
/*!< STM32F10X_LD: STM32 Low density devices */
/* #define STM32F10X_LD_VL */
/*!< STM32F10X_LD_VL: STM32 Low density Value Line devices */
/* #define STM32F10X_MD */
/*!< STM32F10X_MD: STM32 Medium density devices */
/* #define STM32F10X_MD_VL */
/*!< STM32F10X_MD_VL: STM32 Medium density Value Line devices */
/* #define STM32F10X_HD */
/*!< STM32F10X_HD: STM32 High density devices */
/* #define STM32F10X_HD_VL */
/*!< STM32F10X_HD_VL: STM32 High density value line devices */
/* #define STM32F10X_XL */
/*!< STM32F10X_XL: STM32 XL-density devices */
/* #define STM32F10X_CL */
/*!< STM32F10X_CL: STM32 Connectivity line devices */
#endif
2. In file system_stm32f10x.c configure system clock frequency 72MHz-
#if defined (STM32F10X_LD_VL) || (defined STM32F10X_MD_VL) || (defined STM32F10X_HD_VL)
/* #define SYSCLK_FREQ_HSE HSE_VALUE */
#define SYSCLK_FREQ_24MHz 24000000
#else
/* #define SYSCLK_FREQ_HSE HSE_VALUE */
/* #define SYSCLK_FREQ_24MHz 24000000 */
/* #define SYSCLK_FREQ_36MHz 36000000 */
/* #define SYSCLK_FREQ_48MHz 48000000 */
/* #define SYSCLK_FREQ_56MHz 56000000 */
#define SYSCLK_FREQ_72MHz 72000000
#endif
3. Setup your clock as follows--
void
setupClock(
void
)
{
RCC_HCLKConfig(RCC_SYSCLK_Div1);
RCC_PCLK2Config(RCC_HCLK_Div1);
RCC_PCLK1Config(RCC_HCLK_Div2);
FLASH_SetLatency(FLASH_Latency_2);
FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable);
RCC_PLLConfig(RCC_PLLSource_HSE_Div1,RCC_PLLMul_9);
RCC_PLLCmd(ENABLE);
while
(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET) {}
RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);
while
(RCC_GetSYSCLKSource() != 0x08){}
}
2016-02-03 10:46 PM
Hahaha I love this. One issue gets solved and another one crops up! Learning ARM is certainly fun ;p
kk, Thanks for your suggestion. You're a lifesaver. The only reason I was setting up the clocks myself was because I could not figure out why on earth my system_stm32f10x.c was not initializing the clock properly to use HSE and SYSCLK=72Mhz. After breaking my head over it for a day, I gave up and proceeded to set up clocks myself. Although the define in stm32f10x.h should not have any effect on my clock code, based on your suggestion I decided to check it again one last time. This is what I found
#if !defined (STM32F10X_LD) && !defined (STM32F10X_LD_VL) && !defined (STM32F10X_MD) && !defined (STM32F10X_MD_VL) && !defined (STM32F10X_HD) && !defined (STM32F10X_HD_VL) && !defined (STM32F10X_XL) && !defined (STM32F10X_CL)
/* #define STM32F10X_LD */
/*!< STM32F10X_LD: STM32 Low density devices */
/* #define STM32F10X_LD_VL */
/*!< STM32F10X_LD_VL: STM32 Low density Value Line devices */
#define STM32F10X_MD /*!< STM32F10X_MD: STM32 Medium density devices */
/* #define STM32F10X_MD_VL */
/*!< STM32F10X_MD_VL: STM32 Medium density Value Line devices */
/* #define STM32F10X_HD */
/*!< STM32F10X_HD: STM32 High density devices */
/* #define STM32F10X_HD_VL */
/*!< STM32F10X_HD_VL: STM32 High density value line devices */
/* #define STM32F10X_XL */
/*!< STM32F10X_XL: STM32 XL-density devices */
/* #define STM32F10X_CL */
/*!< STM32F10X_CL: STM32 Connectivity line devices */
#endif
Notice how stupidly I had uncommented #define STM32_F10X_MD. I had removed the leading /* but not the trailing */.No wonder my clocks were messed up.
Fixing this and disabling my clock initialization code, gives me the proper clock of SYSCLK=HCLK=72Mhz,
Which creates a new question, What was wrong with my clock initialization code?
2018-12-20 10:04 AM
What about HSE_Config to enable the hse (hse_on)? And I am bit confused about the default state configuration of clock .is it working on internal rc oscillator 8mhz ?
Because as I have checked the default state of clock on stm studio using get_clock function it was showing 72 Mhz using pll.
2018-12-20 12:16 PM
You're digging up an almost 3 year thread, let's not do that. You're arguing with ghosts.
The part starts with the 8 MHz HSI, the PLL from the HSI has a max setting of 64 MHz.
In most cases the SPL implementation should have the clocks enabled/running via the CMSIS SystemInit() function, except for a few broken tool chains. Most often this is a 72 MHz PLL running from an 8 MHz external HSE. Check board for specifics, it is not set in stone.
2018-12-20 7:34 PM
Oh, I have not noticed the post date . Actually I am new to the community and as I found the code for pll and I jumped with my query . I am really sorry for that .
Thanks for your answer and I am implementing cmsis and SPL for codingby using keil ide . I used stm studio for debugging purpose and the value I got 72mhz using pll I am not sure whether it is by hse or hsi.
But anyway your answer is very helpful for me for understanding purpose.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.