2019-01-03 1:06 PM
Hello
I am trying to read the Quadrature optical encoder using TIM2 with STM32F103. I've done the Timer settings. But the TIM2->CNT Always zero. I measured the Timer channels with the oscilloscope. The encoder signals reach TIM_CH1 and TIM_CH2.(PA0, PA1)
This is my init code
void ENCODER_TIM_Init(void){
TIM_Encoder_InitTypeDef TIM_Encoder_Init;
GPIO_InitTypeDef GPIO_InitStruct;
__HAL_RCC_TIM2_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/**TIM2 GPIO Configuration
PA0-WKUP ------> TIM2_CH1
PA1 ------> TIM2_CH2
*/
GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
TIM_Handle.Instance = TIM2;
TIM_Handle.Init.Prescaler = 0;
TIM_Handle.Init.CounterMode = TIM_COUNTERMODE_UP;
TIM_Handle.Init.Period = 0;
TIM_Handle.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
TIM_Encoder_Init.EncoderMode = TIM_ENCODERMODE_TI12;
TIM_Encoder_Init.IC1Polarity = TIM_ICPOLARITY_RISING;
TIM_Encoder_Init.IC1Selection = TIM_ICSELECTION_DIRECTTI;
TIM_Encoder_Init.IC1Prescaler = TIM_ICPSC_DIV1;
TIM_Encoder_Init.IC1Filter = 0x00;
TIM_Encoder_Init.IC2Polarity = TIM_ICPOLARITY_RISING;
TIM_Encoder_Init.IC2Selection = TIM_ICSELECTION_DIRECTTI;
TIM_Encoder_Init.IC2Prescaler = TIM_ICPSC_DIV1;
TIM_Encoder_Init.IC2Filter = 0x00;
if (HAL_TIM_Encoder_Init(&TIM_Handle, &TIM_Encoder_Init) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
if(HAL_TIM_Encoder_Start(&TIM_Handle, TIM_CHANNEL_ALL) != HAL_OK)
{
Error_Handler();
}
}What could be the problem?
Solved! Go to Solution.
2019-01-03 1:47 PM
I solved the problems. I made a mistake timer settings. The TIM period should not be zero.
2019-01-03 1:47 PM
I solved the problems. I made a mistake timer settings. The TIM period should not be zero.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.