2015-06-11 7:41 AM
Hi,
I want to set my RTC alarm sub second with the highest resolution for 1500ms. but there is not any helps, manuals, of sample codes expect ''AN3371 application note''.could any one help me?i realized there isn't function or code inStandard Peripheral Lib.
for sub second alarm. is it?tanx #rtc #stm32f103 #alarm #sub2015-06-11 8:06 AM
1.5 seconds? Is this what you want for you resolution, or alarm interval?
You can change the granularity of the RTC, by changing the prescale divider and select/specify a clock for it.I'm not sure there is a comparator on the subsecond (prescaled) portion of the counter.2015-06-11 8:28 AM
1.5s is the alarm interval, and i want it with the highest resolution.
well, i selected ''LSE'' as clock source. i need it's alarm for wakeup use.tanx for your reply2015-06-11 9:01 AM
Then half the prescaler, and the 32-bit RTC counter will clock at 0.5s intervals, advance the alarm so it wakes every 3 ticks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.