2017-05-18 1:28 AM
Attached :
C2_USB_TEST.ioc
main.c
stm32f1xx_it.c
MCU : STM32F103CBT6
STM32CubeMX : 4.21.0Firmware Package for Family STM32F1 : 1.4.0System Workbench for STM32 - OpenOCD (for Windows 32bits) Version: 1.14.0.201705091103Modifications in main.c :
/* USER CODE BEGIN 0 */ #define RAM_BOOT_LOADER_SIGNATURE_VALUE 0xDEADBEEF #define RAM_BOOT_LOADER_SIGNATURE_ADDRESS 0x20004FF0 void Go_To_ST_Loader() { *((unsigned long *)RAM_BOOT_LOADER_SIGNATURE_ADDRESS) = RAM_BOOT_LOADER_SIGNATURE_VALUE; // 20KB STM32F103 HAL_NVIC_SystemReset(); } //----------------------------------------------------------------------------char usb_buffer[64];
char usb_flag; /* USER CODE END 0 */ /* USER CODE BEGIN 1 */ int l; char x[64]; int i = 0; /* USER CODE END 1 *//* USER CODE BEGIN 2 */
// Activate USB device detection (1.5khoms) HAL_GPIO_WritePin(GPIOA, GPIO_PIN_7, GPIO_PIN_SET); /* USER CODE END 2 *//* USER CODE BEGIN 3 */
if( usb_flag ) { sprintf( x, 'usb:'%.*s'\r\n', usb_flag, usb_buffer ); usb_flag = 0; if( ! memcmp( usb_buffer, 'loader', 6 ) ) { Go_To_ST_Loader(); } CDC_Transmit_FS( x, l ); } else { HAL_Delay(1000); l = sprintf( x, 'cpt = %d\r\n', i++ ); CDC_Transmit_FS( x, l ); }}
/* USER CODE END 3 */Modifications in usbd_cdc_if.c : static int8_t CDC_Receive_FS (uint8_t* Buf, uint32_t *Len) { /* USER CODE BEGIN 6 */ extern char usb_buffer[64]; extern char usb_flag; if(*Len) { usb_flag = *Len; memcpy( usb_buffer, Buf, usb_flag ); } USBD_CDC_SetRxBuffer(&hUsbDeviceFS, &Buf[0]); USBD_CDC_ReceivePacket(&hUsbDeviceFS); return (USBD_OK); /* USER CODE END 6 */ }Windows 10 Microsoft driver 10.0.14393
=> Device detected as : Périphérique série USB (COMn) Results : Usb communication OK in both directions.Same Windows 10 as previous but with ST 'Virtual comport driver' 1.4.0
=> Device detected as : STMicroelectronics Virtual COM Port (COMn) Results : Usb communication OK in both directions.Windows 7 Pro-64 with ST 'Virtual comport driver' 1.4.0
Windows 8.1-64 with ST 'Virtual comport driver' 1.4.0Windows Vista-32 with ST 'Virtual comport driver' 1.4.0 => Device detected as : STMicroelectronics Virtual COM Port (COMn) Results : Usb communication only in one direction PC to Device.I know communication is good in the direction PC to device, because when I send 'loader' to virtual COM port, the device switches to STLoader.
How can I fix this problem ?
Fred.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.