STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 Temperature Function With I/O on PC6

Posted on May 17, 2017 at 07:27 Hello: Question 1: A question that I cannot find an answer for. If I'm using PC6 (STM32F4) as a GPIO already, can I still configure and use the internal temperature sensor on ADC16? Question 2: Using the cal...

STM32CubeMx does not generate syscalls.c

Posted on November 17, 2016 at 08:57Dear all,I have an STM32F746G-DISCO and wanted to get started with printing some text with printf() over the virtual serial COM-port USART1 which is connected via the ST-Link v2.1 with a USB-cable to the PC.I used...

stm32l152 shows cant acess target device.

Posted on May 15, 2017 at 11:52iam working in stm31l152rct6. iam starting to create a iap bootloader (that get from st.com)when programme (FLASH_ProgramHalfPage) reaches half page word write it shows cant acess target device. i don't know whats the ...

alan ajit by Associate II
  • 3450 Views
  • 8 replies
  • 0 kudos

Double Edge PWM: STM32F4 & CubeMX

Posted on May 17, 2017 at 11:16Hi All,I would like to set my STM32F4 Nucleo to do double edge PWM, but for the life of me I cannot figure out how to do it. More specifically I am trying to do it on three channels of TIM1. To put it visually, I am tr...

0690X00000606rzQAA.png
dylan by Associate III
  • 3337 Views
  • 8 replies
  • 0 kudos

How import ''STM32 example'' to System Workbench for STM32 ?

Posted on April 18, 2017 at 16:20Hello,I bought a board STM32F407 Disc1. I wanted to try the example 'Audio_playback_and_record'. But there is not a project for System Workbench for STM32.I opened project in Atollic directory, but I get many errors ...

Peko by Associate III
  • 1662 Views
  • 4 replies
  • 0 kudos

Problem using 32-bit data in internal Flash on STM32F407.

Posted on May 17, 2017 at 16:12Hello.I have problem writing 32-bits word in internal Flash at certain addresses in STM32F407. It is impossible to write 32-bit data at address 0x080E000A. If I try to write data at 0x080F0000 it works perfectly. If I ...

bo2 by Associate
  • 849 Views
  • 2 replies
  • 0 kudos

STM32l1 Nucleo bord using LSE instead of LSI

Posted on May 17, 2017 at 18:24I want to activate the LSE clock on STM32L1 board using processor stm32l152xe on Nucleo board. board  version MB1136 C-03. I far as I can tell no hardware changes required to get the LSE to work.My plan is to run the r...

CAN on STM32F103 RB - Nucleo 64

Posted on May 17, 2017 at 12:00Hi Community, I'm a CAN protocol beginner and I'm quite lost about it. Let’s start from the beginning; I’m working on a CAN bus protocol with two STM32F103 RB – Nucleo 64 microcontrollers and two transceivers MCP2551....

0690X000006071eQAA.png

Resolved! How to activate Compensation Cell on STM32F765?

Posted on May 17, 2017 at 13:45Hallo, on my NUCLEO board with a STM32F765ZI MCU I want to activate the compensation cell.I can do this via* HAL_EnableCompensationCell();* LL_SYSCFG_EnableCompensationCell();* oder manually via** SYSCFG->CMPCR |= SYSC...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.