2016-04-16 2:47 PM
Hello,
I'm working on a cpu intensive project involving CAN bus.
My idea is to use all the 3 available TX mailboxes.
I do my processing, fill up the mailboxes and trigger the transmission. Transmission is started just after filling the relative mailbox
The problem is that all the mailboxes are flagged as successful transmission but i receive only two mailboxes out of 3
It's interesting that the Mailbox relative to the missing message is succesfully transmitted if i set the TIxR.TXRQ in the debugger...I've tried different combinations of IDs:
Test #1:Mailbox 0 -> ID=1 -> ReceivedMailbox 1 -> ID=2 -> Missing
Mailbox 2 -> ID=3 -> Received
Test #2:
Mailbox 0 -> ID=3 -> Received
Mailbox 1 -> ID=2 -> Received
Mailbox 2 -> ID=1 -> Missing
I'm using ABOM and TXFP is disabled. No changes noticed in the behaviour if TXFP enabled.Anyone encountered this behaviour before? Any suggestion?
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.