2021-05-01 4:06 AM
Hi,
I am trying to read HDC1010 temperature sensor with code below, when i click run button while debugging, code does not working, can not continue. But when i debug the function row by row, it woks clearly. Any advise ?
void Receive(u8 Address, u8 Register)
{
/*re-enable ACK bit incase it was disabled last call*/
I2C_AcknowledgeConfig(I2C1, ENABLE);
/* Test on BUSY Flag */
while (I2C_GetFlagStatus(I2C1,I2C_FLAG_BUSY));
/* Enable the I2C peripheral */
/*======================================================*/
I2C_GenerateSTART(I2C1, ENABLE);
/* Test on start flag */
while (!I2C_GetFlagStatus(I2C1,I2C_FLAG_SB));
/* Send device address for write */
I2C_Send7bitAddress(I2C1, Address, I2C_Direction_Transmitter);
/* Test on master Flag */
while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED));
/* Send the device's internal address to write to */
I2C_SendData(I2C1,Register);
/* Test on TXE FLag (data sent) */
while (!I2C_GetFlagStatus(I2C1,I2C_FLAG_TXE));
/*=====================================================*/
/* Send START condition a second time (Re-Start) */
I2C_GenerateSTART(I2C1, ENABLE);
/* Test start flag */
while (!I2C_GetFlagStatus(I2C1,I2C_FLAG_SB));
/* Send address for read */
I2C_Send7bitAddress(I2C1, Address|0x01, I2C_Direction_Receiver);
/* Test Receive mode Flag */
while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_RECEIVER_MODE_SELECTED));
/* load in all 6 registers */
while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_RECEIVED));
data[0] = I2C_ReceiveData(I2C1);
while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_RECEIVED));
data[1] = I2C_ReceiveData(I2C1);
/*enable NACK bit */
I2C_NACKPositionConfig(I2C1, I2C_NACKPosition_Current);
I2C_AcknowledgeConfig(I2C1, DISABLE);
/* Send STOP Condition */
I2C_GenerateSTOP(I2C1, ENABLE);
while(I2C_GetFlagStatus(I2C1, I2C_FLAG_STOPF)); // stop bit flag
}
2021-05-01 12:29 PM
Timing problem?
Sensor conversion time is about 6.5 msec. Do you check the data ready pin before reading?
Cheers, Hal
2021-05-17 5:23 AM
Hi,
Yes i check data ready pin, but i have noticed that there is a problem with stdh peripheral i2c library at startup. Sometimes i get error from while((I2C_GetFlagStatus(I2C_DEV_EEPROM, I2C_FLAG_BUSY) != 0)) and it returns error (but this doesn't occur everytime). So when i try to communicate with HAL library there is no problem. I don't know what is problem with stdh peripheral library.Any advise ?
2021-05-17 8:31 AM
You have apparently isolated the problem to SPL/HDC1010 timing. Perhaps another viewer may have an answer from experience.
Since you seem to prefer the SPL, options to consider:
Cheers, Hal
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.