2016-03-16 11:41 AM
Hello!
I'm trying to connect STM32F103RBT6 to LIS331DLH (accelerometer). LIS331 is connected to PB6/PB7 (I2C1) with pull-up resistors (4K7). STM32CubeMX generated simple code and I added only HAL_I2C_Master_Transmit() function:int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_I
2
C
1
_Init();
result = HAL_I
2
C_Master_Transmit(&hi
2
c
1
,
0
x
30
, sendData,
1
,
2000
);
/* USER CODE BEGIN WHILE */
while (
1
)
{
}
}
The problem is that BUSY flag is alwauys set, so the program can't pass the first while() in function HAL_I2C_Master_Transmit():
if(I
2
C_WaitOnFlagUntilTimeout(hi
2
c, I
2
C_FLAG_BUSY, SET, I
2
C_TIMEOUT_BUSY_FLAG) != HAL_OK)
{
return HAL_BUSY;
}
How can I solve this problem?
Thank you in advance!
2016-03-18 4:32 AM
Hi mt.aveal,
How did you initialize the buffer ''sendData'' ?
-Hannibal-2016-03-18 7:50 AM
Hi! It's simple data buffer:
uint8_t sendData[DATA_SIZE]; sendData[0] = ... sendData[1] = ... sendData[2] = ... I didn't post it, cause I don't think it is a problem. The program doesn't pass to any operations with this buffer.2016-03-20 6:58 AM
It sounds like the SDA or SCL (or both) are being held low. This would cause the peripheral to be in a perpetual busy state. This can be ''real'' and caused by a slave holding one of the signals low or can be ''fake'', caused by buggy silicon as described in the silicon errata in section 2.13.7
http://www.st.com/st-web-ui/static/active/en/resource/technical/document/errata_sheet/CD00190234.pdf
2016-03-20 9:44 AM
Now it passes BUSY flag checking, but stops on:
/* Wait until SB flag is set */
if
(I2C_WaitOnFlagUntilTimeout(hi2c, I2C_FLAG_SB, RESET, Timeout) != HAL_OK)
{
return
HAL_TIMEOUT;
}
The SB is always reset
2016-03-20 10:41 AM
I changed initialization from:
MX_I2C1_Init();
MX_GPIO_Init();
to
MX_GPIO_Init();
MX_I2C1_Init();
And now the program passes SB flag checking and tries to send the address. But I don't see anything on SDA and SCL lines, they are always high...
2016-03-21 5:52 AM
Without knowing what these functions actually do, it's difficult to offer advice. Personally, I would stay right away from the ''Cube'' HAL. As far as making the peripheral operate, there are certain things that must be done:
1. The peripheral clock must be enabled. (RCC->APB1ENR, I2C1EN)2. The pins must be configured as alternate function, open drain.3. The peripheral must be enabled. (I2C1->CR1, PE)Have you chased through the code to see that all this is done properly?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.