2018-09-04 1:15 AM
Hi,
I am working on stm32f100 48 pin device.I am having operational issue while working on usart.
my hw configured to use internal hsi osc which further add pll to generate sysclk of 36Mhz.I am communicating to gsm module over usart3.issue is gsm module not accepting any commands.though i can see responses from module when power on/off.so i tried using loop back test on controller.i found in live watch some data is getting skipped.
other way round i also tested using cp2102 usb to ttl module to check if micro controller transmits command or not.on putty i dont see any commands from controller.
my question---what is maximum clock can be generated using hsi?
how much we can rely on internal osc integrity?? as you suggest some calibration methods
internal osc setting affect baud rate generator?
I have checked gsm module using cp2102 and its working pretty fine.
thanks .
kiran kadam
2018-09-06 10:29 AM
Hi @Community member i would like to show you one analysis.please find below change in usart initialization
this triggers interrupt on receive line continuously.though null bytes stream received.
didn't get this behavior?
USART_DeInit(USART3);
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;//USART_HardwareFlowControl_RTS_CTS;
USART_InitStructure.USART_Mode = USART_Mode_Rx ;//| USART_Mode_Tx;
thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.