2017-03-30 6:42 PM
mcu: stm32f100vct
I am using spi3 and i2c1 together.
However, when i2c1 is used, no signal is output from mosi of spi3.
If i2c1 is deleted, spi3 will operate normally.
If i2c1 and spi1 (remap) are used, I2c SMBA does not work, but spi3 does not work?
If available, please let us know the source.
Thank you.
void SPI3_Init(void)
{
hspi3.Instance = SPI3;
hspi3.Init.Mode = SPI_MODE_MASTER; hspi3.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2; hspi3.Init.NSS = SPI_NSS_SOFT; hspi3.Init.CLKPolarity = SPI_POLARITY_LOW; hspi3.Init.CLKPhase = SPI_PHASE_1EDGE; hspi3.Init.Direction = SPI_DIRECTION_2LINES; hspi3.Init.DataSize = SPI_DATASIZE_8BIT; hspi3.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi3.Init.TIMode = SPI_TIMODE_DISABLE; hspi3.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; // hspi3.Init.CRCPolynomial = 7; HAL_SPI_DeInit(&hspi3); if (HAL_SPI_Init(&hspi3) != HAL_OK) { Error_Handler(); }}
void I2C1_Init(void)
{ hi2c1.Instance = I2C1; hi2c1.Init.ClockSpeed = 400000; hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2; hi2c1.Init.OwnAddress1 = 0; hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT; hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE; hi2c1.Init.OwnAddress2 = 0; hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE; hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE; HAL_I2C_DeInit(&hi2c1); HAL_Delay(5); if (HAL_I2C_Init(&hi2c1) != HAL_OK) { Error_Handler(); } HAL_Delay(5);}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.