2015-10-16 2:07 PM
Using the STM32F072. Have set up the ADC to fire interrupt on end of conversion. It is not firing. I generated code using the latest STM32-CubeMX tool. Attached are resultant adc.c and adc.h. Also attached is full main. Below is pertinent part of main. I set a break-point in ADC1_COMP_IRQHandler() in interrupts.c (also attached) and it never fires. To verify that any interrupts were working I also set a breakpoint at SysTick_Handler() in interrupts.c and it fires fine. Any help would be greatly appreciated.
int main(void){ hal_init(); sysclock_init(); gpio_init(); //adc_init(); MX_ADC_Init(); //McG MX_TIM2_Init(); //mcg __GPIOA_CLK_ENABLE(); //mcg This seems to be missing, can't find it anywhere so we'll do it here. stm32f0xx_hal_adc.c say's we have to. __GPIOB_CLK_ENABLE(); //mcg Ditto HAL_ADC_Start_IT(&hadc); //mcg start ADC in interrupt mode. spi_init(); vhf_init(); uhf_init(); sensors_init(); rs485_init(); gps_init(); ir_efs_init(); // After delay, shut off WS circuit HAL_Delay(100); uint8_t wet_wakeup = HAL_GPIO_ReadPin(WATERSENSE); HAL_GPIO_WritePin(WATERSENSE_ENABLE, GPIO_PIN_SET); if(wet_wakeup) rs485_wakeup(); // Wake up lower units // Start watchdog watchdog_init(); // Software timers uint32_t last_sensors = HAL_GetTick(); uint32_t last_led = HAL_GetTick(); uint32_t last_wakeup = HAL_GetTick(); uint32_t last_engineering = HAL_GetTick(); uint32_t last_rs485_process = HAL_GetTick(); while (1) {....... #stm32-stm32f0-adcWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.