2017-07-05 11:00 PM
Hello everybody,
I am using I2C interface in master mode to collect data from external slave device with DMA in non-blocking mode.
- HAL_I2C_Master_Transmit_DMA
- HAL_I2C_Master_Receive_DMA
My program is working fine since I get correct data.
BUT I would like to get an event that the exchanges are completed by registering these functions during INIT step :
- // HAL Register DMA Tx Transfer events
HAL_DMA_RegisterCallback(dmaHandleTx, HAL_DMA_XFER_CPLT_CB_ID, i2cTransmitFullCallback)- // HAL Register DMA Rx Transfer events
HAL_DMA_RegisterCallback(dmaHandleRx, HAL_DMA_XFER_CPLT_CB_ID, i2cReceiveFullCallback)When I run my program, I get DMA interrupt in below function but no callback call is triggered.
void DMA1_Ch2_3_DMA2_Ch1_2_IRQHandler(void)
{ HAL_DMA_IRQHandler(dmaHandleTx
); HAL_DMA_IRQHandler(dmaHandleRx
);}I tried to look carefully inside the HAL itself and I found something quite strange from my understanding.
HAL_I2C_Master_Transmit_DMA(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint8_t *pData, uint16_t Size)
{ /* Set the I2C DMA transfer complete callback */ hi2c->hdmatx->XferCpltCallback = I2C_DMAMasterTransmitCplt;/* Set the DMA error callback */
hi2c->hdmatx->XferErrorCallback = I2C_DMAError;/* Set the unused DMA callbacks to NULL */
hi2c->hdmatx->XferHalfCpltCallback = NULL; hi2c->hdmatx->XferAbortCallback = NULL;/* Enable the DMA channel */
HAL_DMA_Start_IT(hi2c->hdmatx, (uint32_t)pData, (uint32_t)&hi2c->Instance->TXDR, hi2c->XferSize);}
If the Callback function pointer is initialize at each call of HAL_I2C_Master_Transmit_DMA function with internal I2C_DMAMasterTransmitCplt, how it manages my registered callback in INIT step (i2cTransmitFullCallback) ?
Does anyone has an idea about this ?
Thanks a lot.
Solved! Go to Solution.
2017-07-07 2:47 AM
hi, if you just want callbacks after HAL_I2C_Master_Transmit_DMA and HAL_I2C_Master_Receive_DMA routines,
You just need to implement your
void HAL_I2C_MasterTxCpltCallback(I2C_HandleTypeDef *hi2c);
void HAL_I2C_MasterRxCpltCallback(I2C_HandleTypeDef *hi2c);
they are weakly defined in stm32f0xx_hal_i2c.c,
Don't forget to enable I2Cx event global interrupt. So that in your stm32f0xx_it.c,
you will see something like
void I2Cx_IRQHandler(void)
{
HAL_I2C_EV_IRQHandler(&I2cHandle);
HAL_I2C_ER_IRQHandler(&I2cHandle);
}
Good Luck!
2017-07-07 2:47 AM
hi, if you just want callbacks after HAL_I2C_Master_Transmit_DMA and HAL_I2C_Master_Receive_DMA routines,
You just need to implement your
void HAL_I2C_MasterTxCpltCallback(I2C_HandleTypeDef *hi2c);
void HAL_I2C_MasterRxCpltCallback(I2C_HandleTypeDef *hi2c);
they are weakly defined in stm32f0xx_hal_i2c.c,
Don't forget to enable I2Cx event global interrupt. So that in your stm32f0xx_it.c,
you will see something like
void I2Cx_IRQHandler(void)
{
HAL_I2C_EV_IRQHandler(&I2cHandle);
HAL_I2C_ER_IRQHandler(&I2cHandle);
}
Good Luck!
2017-07-07 9:06 AM
Hi Zhitai Liu,
Thanks for your support Now I get interrupt callback to my upper layer.
Using:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.