2018-01-03 6:32 AM
Hi,
For few days I am trying to get my PWM generator works under TIM1. I cannot find what is wrong but counter seems to work but no output is available under GPIO_A8 pin.
Configuration code looks like:
static void
MX_TIM1_Init(void
){LL_TIM_InitTypeDef
TIM_InitStruct;
LL_TIM_OC_InitTypeDef
TIM_OC_InitStruct;
LL_TIM_BDTR_InitTypeDef
TIM_BDTRInitStruct;
LL_GPIO_InitTypeDef
GPIO_InitStruct;
/* Peripheral clock enable */
LL_APB1_GRP2_EnableClock(
LL_APB1_GRP2_PERIPH_TIM1
);
TIM_InitStruct.
Prescaler
=600
;
TIM_InitStruct.
CounterMode
=LL_TIM_COUNTERMODE_UP
;
TIM_InitStruct.
Autoreload
=400
;
TIM_InitStruct.
ClockDivision
=LL_TIM_CLOCKDIVISION_DIV4
;
TIM_InitStruct.
RepetitionCounter
=1
;
LL_TIM_Init(
TIM1
,
&TIM_InitStruct);
LL_TIM_EnableARRPreload(
TIM1
);
LL_TIM_SetClockSource(
TIM1
,
LL_TIM_CLOCKSOURCE_INTERNAL
);
LL_TIM_OC_EnablePreload(
TIM1
,
LL_TIM_CHANNEL_CH1
);
TIM_OC_InitStruct.
OCMode
=LL_TIM_OCMODE_PWM1
;
TIM_OC_InitStruct.
OCState
=LL_TIM_OCSTATE_DISABLE
;
TIM_OC_InitStruct.
OCNState
=LL_TIM_OCSTATE_DISABLE
;
TIM_OC_InitStruct.
CompareValue
=200
;
TIM_OC_InitStruct.
OCPolarity
=LL_TIM_OCPOLARITY_HIGH
;
TIM_OC_InitStruct.
OCNPolarity
=LL_TIM_OCPOLARITY_HIGH
;
TIM_OC_InitStruct.
OCIdleState
=LL_TIM_OCIDLESTATE_HIGH
;
//LL_TIM_OCIDLESTATE_LOW;
TIM_OC_InitStruct.
OCNIdleState
=LL_TIM_OCIDLESTATE_LOW
;
LL_TIM_OC_Init(
TIM1
,
LL_TIM_CHANNEL_CH1
,
&TIM_OC_InitStruct);
LL_TIM_OC_DisableFast(
TIM1
,
LL_TIM_CHANNEL_CH1
);
LL_TIM_SetTriggerOutput(
TIM1
,
LL_TIM_TRGO_RESET
);
LL_TIM_DisableMasterSlaveMode(
TIM1
);
// TIM_BDTRInitStruct.OSSRState = LL_TIM_OSSR_DISABLE;
// TIM_BDTRInitStruct.OSSIState = LL_TIM_OSSI_DISABLE;
// TIM_BDTRInitStruct.LockLevel = LL_TIM_LOCKLEVEL_OFF;
// TIM_BDTRInitStruct.DeadTime = 0;
// TIM_BDTRInitStruct.BreakState = LL_TIM_BREAK_DISABLE;
// TIM_BDTRInitStruct.BreakPolarity = LL_TIM_BREAK_POLARITY_HIGH;
// TIM_BDTRInitStruct.AutomaticOutput = LL_TIM_AUTOMATICOUTPUT_DISABLE;
// LL_TIM_BDTR_Init(TIM1, &TIM_BDTRInitStruct);
/**TIM1 GPIO Configuration
PA8 ------> TIM1_CH1
*/
// GPIO_InitStruct.Pin = LL_GPIO_PIN_8;
// GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
// GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH;
// GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
// GPIO_InitStruct.Pull = LL_GPIO_PULL_DOWN; //LL_GPIO_PULL_NO;
// GPIO_InitStruct.Alternate = LL_GPIO_AF_2;
// LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
LL_AHB1_GRP1_EnableClock(
LL_AHB1_GRP1_PERIPH_GPIOA
);
LL_GPIO_SetPinMode(
GPIOA
,
LL_GPIO_PIN_8
,
LL_GPIO_MODE_ALTERNATE
);
LL_GPIO_SetPinPull(
GPIOA
,
LL_GPIO_PIN_8
,
LL_GPIO_PULL_NO
);
LL_GPIO_SetPinSpeed(
GPIOA
,
LL_GPIO_PIN_8
,
LL_GPIO_SPEED_FREQ_HIGH
);
LL_GPIO_SetAFPin_8_15(
GPIOA
,
LL_GPIO_PIN_8
,
LL_GPIO_AF_2
);
LL_TIM_OC_SetCompareCH1(
TIM1
,
200
);
LL_TIM_CC_EnableChannel(
TIM1
,
LL_TIM_CHANNEL_CH1
);
LL_TIM_OC_SetMode(
TIM1
,
LL_TIM_CHANNEL_CH1
,
LL_TIM_OCMODE_PWM1
);
LL_TIM_GenerateEvent_UPDATE(
TIM1
);
LL_TIM_EnableCounter(
TIM1
);
}And it is invoked inside main loop:
int
main(void
){ LL_Init();
SystemClock_Config()
;
MX_TIM1_Init()
;
while(1);}And System Clock config:
void
SystemClock_Config(void
){ LL_FLASH_SetLatency(LL_FLASH_LATENCY_1
);
if
(LL_FLASH_GetLatency() !=LL_FLASH_LATENCY_1
) {Error_Handler
();
} LL_RCC_HSI_Enable()
;
/* Wait till HSI is ready */
while
(LL_RCC_HSI_IsReady() !=1
) { } LL_RCC_HSI_SetCalibTrimming(16
);
LL_RCC_PLL_ConfigDomain_SYS(
LL_RCC_PLLSOURCE_HSI
,
LL_RCC_PLL_MUL_12
,
LL_RCC_PREDIV_DIV_2
);
LL_RCC_PLL_Enable()
;
/* Wait till PLL is ready */
while
(LL_RCC_PLL_IsReady() !=1
) { } LL_RCC_SetAHBPrescaler(LL_RCC_SYSCLK_DIV_1
);
LL_RCC_SetAPB1Prescaler(
LL_RCC_APB1_DIV_1
);
LL_RCC_SetSysClkSource(
LL_RCC_SYS_CLKSOURCE_PLL
);
/* Wait till System clock is ready */
while
(LL_RCC_GetSysClkSource() !=LL_RCC_SYS_CLKSOURCE_STATUS_PLL
) { } LL_Init1msTick(48000000
);
LL_SYSTICK_SetClkSource(
LL_SYSTICK_CLKSOURCE_HCLK
);
LL_SetSystemCoreClock(
48000000
);
LL_RCC_SetUSARTClockSource(
LL_RCC_USART2_CLKSOURCE_PCLK1
);
/* SysTick_IRQn interrupt configuration */
NVIC_SetPriority(
SysTick_IRQn
,
0
);
}Can anyone deal with that issue?
#pwm #stm32f072 #timer12018-01-03 6:45 AM
I don't Cube, but do you set TIMx_BDTR.MOE?
JW
2018-01-03 7:07 AM
In SPL you had to enable PWM Output on TIM1/TIM8
/**
* @brief Enables or disables the TIM peripheral Main Outputs. * @param TIMx: where x can be 1 or 8 to select the TIMx peripheral. * @param NewState: new state of the TIM peripheral Main Outputs. * This parameter can be: ENABLE or DISABLE. * @retval None */void TIM_CtrlPWMOutputs(TIM_TypeDef* TIMx, FunctionalState NewState){ /* Check the parameters */ assert_param(IS_TIM_LIST4_PERIPH(TIMx)); assert_param(IS_FUNCTIONAL_STATE(NewState));if (NewState != DISABLE)
{ /* Enable the TIM Main Output */ TIMx->BDTR |= TIM_BDTR_MOE; } else { /* Disable the TIM Main Output */ TIMx->BDTR &= (uint16_t)~TIM_BDTR_MOE; }}In HAL you need to check
LL_TIM_EnableAllOutputs()
/**
* @brief Enable the outputs (set the MOE bit in TIMx_BDTR register).
* @note The MOE bit in TIMx_BDTR register allows to enable /disable the outputs by * software and is reset in case of break or break2 event * @note Macro @ref IS_TIM_BREAK_INSTANCE(TIMx) can be used to check whether or not * a timer instance provides a break input. * @rmtoll BDTR MOE LL_TIM_EnableAllOutputs * @param TIMx Timer instance * @retval None */__STATIC_INLINE void LL_TIM_EnableAllOutputs(TIM_TypeDef *TIMx){ SET_BIT(TIMx->BDTR, TIM_BDTR_MOE);}2018-01-11 9:12 AM
In main.c file, in function SystemClock_Config,insert the following line as the first code line in the function and see if is working...
LL_FLASH_Enable64bitAccess();
�?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.