2015-11-30 4:35 PM
I have set the data size to 8 bits for SPI on SPI1 using the pins PB3,4,5, PA15.
I see 8 bits of data on the MOSI line corresponding to the 8 bits I put into SPI1-DR. But on the rx side I see the 8 rx bits in SPI-DR [15:8] followed by 0 in [7:0]. I have altered my library call to read all 16 bits and then right shift to get the 8 bits in the MSB byte and return it as the read data. But according to the documentation that should be WRONG. Here are the SPI registers just before I pop the value from DR. SPI1->CR1= 0x35C SPI1->CR2=0x1704 SPI1->SR = 0x203 I am at a loss to explain it. #stm32f05-spiWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.