2018-03-09 4:19 AM
I have been trying to use the USART idle line detection flag to detect when an incoming transmission stream has ended.
if
((USART1->
ISR&
USART_ISR_RXNE)!=
RESET) {if
((1+
RX_BUFFER_POS)<
RX_BUFFER_SIZE) { RX_Buffer[1
+
RX_BUFFER_POS++
]=
USART1->
RDR; } }if
(__HAL_UART_GET_FLAG(&
huart1,UART_FLAG_IDLE)) { can_read=
1
; __HAL_UART_CLEAR_FLAG(&
huart1, UART_FLAG_IDLE); }I used this code to set a flag, can_read which is checked in the main loop. If the flag is true, then I parse the data.
The problem is that the IDLE flag is being set after each character received, not after the end of the string.
Please can I have some clarification on when the IDLE interrupt is triggered.
Many thanks.
#hal-usart #usart-idle #usart-pins2018-03-09 4:45 AM
Hello
tomeaton17
,You if statement checks only if there is byte ready to read.
IDLE line event is triggered if UART RX line is inactive for one frame. The frame time depends on your baudrate. Higher baudrate, lower frame.
You should not use IDLE line to detect end of string. You should use IDLE line to detect IDLE line only and then check if you have entire string already received. To detect end of string, you should (in most cases) wait for line feed(LF) character or carriage return (CR).
Please check
for more information.Best regards,
Tilen
2018-03-09 4:54 AM
when the IDLE interrupt is triggered
RM0090 says:
An Idle character is interpreted as an entire frame of “1�s
followed by the start bit of the
next frame
which contains data (The number of “1� ‘s will include the number of stop bits).(my emphasis)
2018-03-09 7:02 AM
I use a circular DMA buffer;
if (HAL_UART_Receive_DMA(&huart4, (uint8_t *)Usart3RxDMABuffer, U3RxBufSize) != HAL_OK)
_Error_Handler(__FILE__, __LINE__);
char readableU3(void) {
U3RxBufferPtrIN = U3RxBufSize - huart4.hdmarx->Instance->CNDTR; return U3RxBufferPtrIN - U3RxBufferPtrOUT;}char getc3(void) {
char Rxbyte = Usart3RxDMABuffer[U3RxBufferPtrOUT++]; if (U3RxBufferPtrOUT >= U3RxBufSize) U3RxBufferPtrOUT = 0; return Rxbyte;}usage:
(every mS)
{
if (readableU3() >= LoRaPacketLength) // have packet end <- polling of buffer size, waiting for packet length
{ haveLoraMessageinRxTable = true; // flag foreground to process LoRa Rx Framefor (int i = 0; i < LoRaPacketLength; i++) // copy away frame contents for later processing
LoRaRxFrames[LoRaRxFrameIn][i] = getc3(); . }.
.}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.