2014-10-31 1:24 PM
I have a strange problem. I use the code below on the STM32F05 series and it works just fine. Transfer it to the STM32F072 and it does not work. When applying voltage to any given port, the ADC readings change on multiple ports. Voltage reference is stable. Any idea why this would happen?
//Use the follwing code for interrupts for DMA tranfer complete interrupt and half tranfer interrupt complete. //NVIC_InitTypeDef NVIC_InitStructure; // Enable and set DMA1_Channel1 Interrupt */ //NVIC_InitStructure.NVIC_IRQChannel = DMA1_Channel1_IRQn; //NVIC_InitStructure.NVIC_IRQChannelPriority = 0x00; //NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; //NVIC_Init(&NVIC_InitStructure); // Enable DMA1 Channel1 Half Transfer and Transfer Complete interrupt // DMA_ITConfig(DMA1_Channel1, DMA_IT_HT, ENABLE); // DMA_ITConfig(DMA1_Channel1, DMA_IT_TC, ENABLE); /* GPIOA Periph clock enable */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); GPIO_InitTypeDef GPIO_InitStructure; /* Configure ADC Channels as analog input - might conflict */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin_4; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure); TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_OCInitTypeDef TIM_OCInitStructure; ADC_InitTypeDef ADC_InitStructure; DMA_InitTypeDef DMA_InitStructure; /* ADC1 DeInit */ ADC_DeInit(ADC1); /* ADC1 Periph clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1 | RCC_APB2Periph_TIM1, ENABLE); /* DMA1 clock enable */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE); /* TIM2 Configuration */ TIM_DeInit(TIM1); /* Time base configuration */ TIM_TimeBaseStructInit(&TIM_TimeBaseStructure); TIM_TimeBaseStructure.TIM_Prescaler = (SystemCoreClock / 1000000) - 1; // 1 MHz, from 48 MHz TIM_TimeBaseStructure.TIM_Period = 500 - 1; // 2 KHz TIM_TimeBaseStructure.TIM_ClockDivision = 0x0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure); /* Output Compare PWM Mode configuration */ TIM_OCStructInit(&TIM_OCInitStructure); TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; /* low edge by default */ TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = 0x01; TIM_OC4Init(TIM1, &TIM_OCInitStructure); /* TIM1 enable counter */ TIM_Cmd(TIM1, ENABLE); /* Main Output Enable */ TIM_CtrlPWMOutputs(TIM1, ENABLE); /* DMA1 Channel1 Config */ DMA_DeInit(DMA1_Channel1); DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR; DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&RegularConvData[0]; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC; DMA_InitStructure.DMA_BufferSize = SAMPLES; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; DMA_Init(DMA1_Channel1, &DMA_InitStructure); /* DMA1 Channel1 enable */ DMA_Cmd(DMA1_Channel1, ENABLE); /* ADC DMA request in circular mode */ ADC_DMARequestModeConfig(ADC1, ADC_DMAMode_Circular); /* Enable ADC_DMA */ ADC_DMACmd(ADC1, ENABLE); /* Initialize ADC structure */ ADC_StructInit(&ADC_InitStructure); /* Configure the ADC1 in continous mode withe a resolutuion equal to 12 bits */ ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; ADC_InitStructure.ADC_ContinuousConvMode = DISABLE; ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_Rising; ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC4; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_ScanDirection = ADC_ScanDirection_Upward; ADC_Init(ADC1, &ADC_InitStructure); /* Convert the ADC_Channnel_0 with 7.5 Cycles as sampling time */ ADC_ChannelConfig(ADC1, ADC_Channel_0 , ADC_SampleTime_239_5Cycles); /* Convert the ADC_Channnel_1 with 7.5 Cycles as sampling time */ ADC_ChannelConfig(ADC1, ADC_Channel_1 , ADC_SampleTime_239_5Cycles); /* Convert the ADC_Channnel_2 with 7.5 Cycles as sampling time */ ADC_ChannelConfig(ADC1, ADC_Channel_2 , ADC_SampleTime_239_5Cycles); /* Convert the ADC_Channnel_3 with 7.5 Cycles as sampling time */ ADC_ChannelConfig(ADC1, ADC_Channel_3 , ADC_SampleTime_239_5Cycles); /* Convert the ADC_Channnel_4 with 7.5 Cycles as sampling time */ ADC_ChannelConfig(ADC1, ADC_Channel_4 , ADC_SampleTime_239_5Cycles); /* ADC Calibration */ ADC_GetCalibrationFactor(ADC1); /* Enable ADC1 */ ADC_Cmd(ADC1, ENABLE); /* Wait the ADCEN flag */ while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_ADEN)); /* ADC1 regular Software Start Conv */ ADC_StartOfConversion(ADC1); return;2014-11-03 2:20 PM
Problem solved. Code above works fine. Grounding issues from unstable split supplies.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.