2014-06-22 8:32 AM
Hello
Does anyone have working initialization code for STM32F042?I wrote this one bellow, but it doesn't work and I dont know why? CAN_TX line is low (measured by means of oscilloscope).I have got simillar working code for stm32f103c6t6.void CAN_init(void){ GPIO_InitTypeDef GPIO_InitStructure; RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1,ENABLE); //CAN TX RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOA, &GPIO_InitStructure); //CAN RX GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN; //GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOA, &GPIO_InitStructure); NVIC_InitTypeDef NVIC_InitStructure; /* Enable CAN1 RX0 interrupt IRQ channel */ NVIC_InitStructure.NVIC_IRQChannel = CEC_CAN_IRQn; NVIC_InitStructure.NVIC_IRQChannelPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); CAN_InitTypeDef CAN_InitStructure; /* CAN register init */ CAN_DeInit( CAN1); CAN_StructInit(&CAN_InitStructure); /* CAN cell init */ CAN_InitStructure.CAN_TTCM = DISABLE; CAN_InitStructure.CAN_ABOM = DISABLE; CAN_InitStructure.CAN_AWUM = DISABLE; CAN_InitStructure.CAN_NART = DISABLE; CAN_InitStructure.CAN_RFLM = DISABLE; CAN_InitStructure.CAN_TXFP = DISABLE; CAN_InitStructure.CAN_Mode = CAN_Mode_Normal; CAN_InitStructure.CAN_SJW = CAN_SJW_1tq; CAN_InitStructure.CAN_BS1 = CAN_BS1_8tq; CAN_InitStructure.CAN_BS2 = CAN_BS2_7tq; CAN_InitStructure.CAN_Prescaler = 2; CAN_Init(CAN1, &CAN_InitStructure); /* CAN filter init */ CAN_FilterInitTypeDef CAN_FilterInitStructure; CAN_FilterInitStructure.CAN_FilterNumber = 1; CAN_FilterInitStructure.CAN_FilterMode = CAN_FilterMode_IdMask; CAN_FilterInitStructure.CAN_FilterScale = CAN_FilterScale_32bit; CAN_FilterInitStructure.CAN_FilterIdHigh = 0x0000; CAN_FilterInitStructure.CAN_FilterIdLow = 0x0000; CAN_FilterInitStructure.CAN_FilterMaskIdHigh = 0x0000; CAN_FilterInitStructure.CAN_FilterMaskIdLow = 0x0000; CAN_FilterInitStructure.CAN_FilterFIFOAssignment = CAN_FIFO0; CAN_FilterInitStructure.CAN_FilterActivation = ENABLE; CAN_FilterInit(&CAN_FilterInitStructure); /* CAN FIFO0 message pending interrupt enable */ CAN_ITConfig(CAN1, CAN_IT_FMP0, ENABLE); /* transmit 1 message */ CanTxMsg TxMessage; TxMessage.StdId = 0x7ff; //TxMessage.ExtId = 0x7f7f; TxMessage.IDE = CAN_ID_STD; TxMessage.RTR = CAN_RTR_DATA; TxMessage.DLC = 0; TxMessage.Data[0] = 0xDE; TxMessage.Data[1] = 0xCA; CAN_Transmit(CAN1, &TxMessage);}Can anyone help?Best regardsJanusz Brela2014-06-22 1:23 PM
Would you need to use GPIO_PinAFConfig() to configure the specific peripheral functionality?
2014-06-22 1:30 PM
STM32F0xx_StdPeriph_Lib_V1.3.1\Projects\STM32F0xx_StdPeriph_Examples\CAN\CAN_Networking\main.c
http://www.st.com/web/en/catalog/tools/PF257884
2014-06-23 5:03 AM
I'll check it.
Thanks a lot, I could not find good examples o ST web site.Best RegardsJanusz BrelaWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.