2017-08-15 10:55 AM
Hello.
I am using a stm32F042 for some CAN communications, alongside a SN65HVD230 as transceiver.
I have two boards (my own) using both those ICs.
I made a simple program, based on the STM32 example, from a STMCube initial code.
Actually, i have problems making my two modules discussing. Sending � works � (in the way that the can outputs things), but receiving does not.
I�ll go into code later eventually, but i first have a question about what the STM32F outputs. Please see the CAN oscilloscope trace below. CAN_L and CAN_H signals are cyan and yellow, blue is what comes out of the transceiver on receiving side.
This signal is generated, then the sender enters timeout. It seems there are a dozen attempts, then a burst of much shorter pikes.
What bothers me is that i cannot relate this signal to anything i could gather from docs, like the CAN frame description..
At the moment, i do believe the receiver does not understand the data that is sent, as it looks like garbage to me.
Any idea, please?
#problem #canWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.