2020-02-16 10:49 PM
Hi, I'm using stm32f030cct6 and control the sx1276.
I configured SPI1 like that
void SPI1_Init(void)
{
SPI_InitTypeDef SPI_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA | RCC_AHBPeriph_GPIOB, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);
/*****************MOSI, MISO SCLK GPIO Config********************/
/**SPI1 GPIO Configuration
PB3 ------> SPI1_SCK
PB4 ------> SPI1_MISO
PB5 ------> SPI1_MOSI
*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3 | GPIO_Pin_4 | GPIO_Pin_5;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOB, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOB,GPIO_PinSource3,GPIO_AF_0);
GPIO_PinAFConfig(GPIOB,GPIO_PinSource4,GPIO_AF_0);
GPIO_PinAFConfig(GPIOB,GPIO_PinSource5,GPIO_AF_0);
/******************Chip Select GPIO Config**********************/
//RF_NSS
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_SetBits(GPIOA,GPIO_Pin_15);
/******************SPI1 Config for SX1276************************/
SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
SPI_InitStructure.SPI_Mode = SPI_Mode_Master;
SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;
SPI_InitStructure.SPI_CPOL = SPI_CPOL_Low;
SPI_InitStructure.SPI_CPHA = SPI_CPHA_1Edge;
SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;
SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_16; // 5 MHz
//SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_8; // 10 MHz
SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;
SPI_InitStructure.SPI_CRCPolynomial = 7;
SPI_Init(SPI1, &SPI_InitStructure);
SPI_Cmd(SPI1, ENABLE);
}
and send data to sx1276, but occured problem.
uint8_t SpiInOut( uint8_t outData )
{
/* Send SPIy data */
SPI_SendData8( SPI1, outData );
while( SPI_I2S_GetFlagStatus( SPI1, SPI_I2S_FLAG_RXNE ) == RESET );
return SPI_ReceiveData8( SPI1 );
}
in that fucntion, SPI1->SR register is 0x202 so I can't receive data.
what's the problem?, what should i do?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.