2017-11-04 3:50 AM
hello
I have stm32f030f4p6 Microcontroller and using iar Compiler , library cmsis , After confige Uart1 the RXNE , FE and CMF bits return 1 whereas not recieve or send was done if I dont set RXNE bit to 0 thats Stuck on interrupt routine And that recieve nothing here is my Uart Config:
USART1->BRR = 0x1388; USART1->CR1 = USART_CR1_UE | USART_CR1_TE | USART_CR1_RE; and GPIO config and Nvic:
NVIC_InitTypeDef NVIC_InitStructure; USART1->CR1 |= USART_CR1_RXNEIE; NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn; NVIC_InitStructure.NVIC_IRQChannelPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure);
and the register after this 2 line USART1->BRR = 0x1388; USART1->CR1 = USART_CR1_UE | USART_CR1_TE | USART_CR1_RE;
http://s9.picofile.com/file/8310890334/photo_2017_11_04_14_10_29.jpg
rx tx connected to sim800 module and its answer to AT Properly
thank you
#stm32f0 #rx #interrupt #usartWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.