2017-04-14 5:44 AM
i'm trying to communicate with NRF24L01 RFmodule, it seems that spi init. is ok , but when i'm trying to read for example theREG_RF_CH Registry (0x05) it should return the reset value (0x02) but that does not happen !! it return 0x00 for the first time then atthe second time i trying to read the same registry it return the correct value!! i assume that the RX FIFO store the value at first time then give me it in the second time !!
my code as below:static void SPI1_Init(void){
RCC->AHBENR |= RCC_AHBENR_GPIOAEN; /* Enable GPIOA clock */
RCC->AHBENR |= RCC_AHBENR_GPIOBEN; /* Enable GPIOB clock */
RCC->APB2ENR |= RCC_APB2ENR_SPI1EN; /* Enable SPI1 clock */
/* Configure PA6 to MISO, PA7 to MOSI, PB3 to SCK */
GPIOA->AFR[0] &= ~((15ul << 4* 6) | (15ul << 4* 7));
GPIOA->AFR[0] |= (( 0ul << 4* 6) | ( 0ul << 4* 7));
GPIOB->AFR[0] &= ~(15ul << 4* 3);
GPIOB->AFR[0] |= ( 0ul << 4* 3);
GPIOA->MODER &= ~(( 3ul << 2* 6) | ( 3ul << 2* 7));
GPIOA->MODER |= (( 2ul << 2* 6) | ( 2ul << 2* 7));
GPIOB->MODER &= ~( 3ul << 2* 3);
GPIOB->MODER |= ( 2ul << 2* 3);
SPI1->CR1 = 0x00000000; /* Reset SPI1 CR1 Registry*/
SPI1->CR1 = (( 0ul << 0) | /* CPHA=0 */
( 0ul << 1) | /* CPOL=0 */
( 1ul << 2) | /* MSTR=1 */
( 4ul << 3) | /* BR (fPCLK/32) ~= 1.5 Mbit/sec */
( 0ul << 7) | /* LSBFIRST */
( 0ul << 8) | /* SSI */
( 1ul << 9)); /* SSM */
SPI1->CR2 = 0x00000000; /* Reset SPI1 CR2 Registry*/
SPI1->CR2 |= (SPI_CR2_NSSP | SPI_CR2_DS_0 | SPI_CR2_DS_1 | SPI_CR2_DS_2 | SPI_CR2_FRXTH);
SPI1->CRCPR = 0x0007;
SPI1->CR1 |= SPI_CR1_SPE; /* Enable SPI1 */
}
uint8_t SPI1_WriteRead_byte (uint8_t wr) {
uint8_t data=0;
while ((SPI1->SR & SPI_SR_TXE) != SPI_SR_TXE);
*(uint8_t *)&(SPI1->DR) = wr;
data = SPI1->DR;
return data;
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
#spi #stm32-f0
Solved! Go to Solution.
2017-04-14 9:29 AM
First, if it is byte communication, when reading, make sure it is an 8 bit read
before
data = SPI1->DR; after data = *(uint8_t *)&(SPI1->DR);When the communication starts, the SPI is waiting to send data (TXE=1)... and at that time, there is nothing yet to read, until 8 SPI SCK clock pulses have been generated. Then RXNE = 1 and DR can be read.
Try to wait for RXNE flag before reading the received data.
If that works, then next step will be to wonder how not to pause the SPI clock between bytes...
2017-04-14 9:29 AM
First, if it is byte communication, when reading, make sure it is an 8 bit read
before
data = SPI1->DR; after data = *(uint8_t *)&(SPI1->DR);When the communication starts, the SPI is waiting to send data (TXE=1)... and at that time, there is nothing yet to read, until 8 SPI SCK clock pulses have been generated. Then RXNE = 1 and DR can be read.
Try to wait for RXNE flag before reading the received data.
If that works, then next step will be to wonder how not to pause the SPI clock between bytes...
2017-04-17 10:06 AM
Thanks
Centauris.Alpha
for your Help, you are right, the correct code is: uint8_t SPI1_WriteRead_byte (uint8_t wr) {uint8_t data=0;
while ((SPI1->SR & SPI_SR_TXE) != SPI_SR_TXE); *((__IO uint8_t *)&SPI1->DR) = wr; while ((SPI1->SR & SPI_SR_BSY) == SPI_SR_BSY); while ((SPI1->SR & SPI_SR_RXNE) != SPI_SR_RXNE); data = *((__IO uint8_t *)&SPI1->DR); return data; }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.