2016-10-27 4:34 AM
Hello,
I'm using a stm32f030x6. During normal operation i need my swclk-pin (PA14 in my package) to be configured as a UART. However for debugging, i'd like to reconfigure it back and use it as a swclk to use it with the ST-LINK i tried the following: void ReEnableSWCLK() { GPIO_InitTypeDef GPIO_InitStruct; GPIO_InitStruct.Pin = GPIO_PIN_14; // only initialize the CLK GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLDOWN; GPIO_InitStruct.Speed = GPIO_SPEED_LOW; GPIO_InitStruct.Alternate = GPIO_AF0_SWCLK; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); } which did not work. Then Resetting the whole GPIOA registers back to their reset values (then SWD is available): // bring back the SWD port! GPIOA->AFR[0] = 0x00000000; GPIOA->AFR[1] = 0x00000000; GPIOA->MODER = 0x28000000; GPIOA->OTYPER = 0x00000000; GPIOA->OSPEEDR = 0x0C000000; GPIOA->PUPDR = 0x24000000; which sort o helps: my st-link finds the chip (unlike in uart mode) but it fails to really comunicate to it: Info : using stlink api v2 Info : Target voltage: 3.592147 Info : stm32f0x.cpu: hardware has 4 breakpoints, 2 watchpoints Error: jtag status contains invalid mode value - communication failure Polling target stm32f0x.cpu failed, trying to reexamine Info : stm32f0x.cpu: hardware has 4 breakpoints, 2 watchpoints Info : Previous state query failed, trying to reconnect Error: jtag status contains invalid mode value - communication failure and so on... i'm tying to reenable the swclk from an interrupt routine. Any Idea what's going wrong? any help is higly appreciated. Thank you!! #stm32f030-!swclk2016-10-27 5:00 AM
Ha figured out what the problem was: someone else was spamming my port. so it kept disconnecting. last approach works! (maybe first aswell)
SOLVEDWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.