2012-10-07 7:57 AM
So I managed to get my boards programmed and working... except one little detail - power consumption is rather high for my application. With both UARTs on and nothing else, running on HSI at 48Mhz, current consumption is at 10.2mA when starting up and 9.5-9.3 once everything is initialized.
Any suggestions towards lowering that? Ideally under 5mA... if that's even possible?Would hate having to switch to STM32L* now that all code was done? TIA!2012-10-10 3:34 AM
You may be right, the cpu core uses all four cycles to process single instruction, really simple cpu.
I understand ''really simple cpu'' as euphemism for ''botched''. I have to work with this thing, which is not really funny...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.